Status
Alarms Status
The alarms status register indicates the current status of the alarms:
-
alarm bit = 0: alarm is not active.
-
alarm bit = 1: alarm is active.
The following table describes the values for each bit of the alarm status register:
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Bit |
Description |
---|---|---|---|---|---|---|---|---|---|
0x1647 |
5704 |
R |
– |
– |
INT16U |
– |
A/E |
– |
Alarm status |
A/E |
0 |
User-defined alarm 201 |
|||||||
A/E |
1 |
User-defined alarm 202 |
|||||||
A/E |
2 |
User-defined alarm 203 |
|||||||
A/E |
3 |
User-defined alarm 204 |
|||||||
A/E |
4 |
User-defined alarm 205 |
|||||||
A/E |
5 |
User-defined alarm 206 |
|||||||
A/E |
6 |
User-defined alarm 207 |
|||||||
A/E |
7 |
User-defined alarm 208 |
|||||||
A/E |
8 |
User-defined alarm 209 |
|||||||
A/E |
9 |
User-defined alarm 210 |
|||||||
A/E |
10 |
Long-time protection Ir pre-alarm (PAL Ir) |
|||||||
E |
11 |
Earth-leakage protection IΔn pre-alarm (PAL IΔn) |
|||||||
A/E |
12 |
Ground-fault protection Ig pre-alarm (PAL Ig) |
|||||||
– |
13–15 |
Reserved |
SDx Module Status
The SDx module status register indicates the status and the validity of the SDx outputs (2 outputs maximum):
-
status bit = 0: the output is open.
-
status bit = 1: the output is closed.
-
validity bit = 0: the output status is unknown.
-
validity bit = 1: the output status is known.
The following table describes the values for each bit of the SDx module status register:
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Bit |
Description |
---|---|---|---|---|---|---|---|---|---|
0x2298 |
8857 |
R |
– |
– |
INT16U |
– |
A/E |
– |
SDx module status |
A/E |
0 |
Status of output 1 |
|||||||
A/E |
1 |
Status of output 2 |
|||||||
– |
2–7 |
Reserved |
|||||||
A/E |
8 |
Validity of output 1 |
|||||||
A/E |
9 |
Validity of output 2 |
|||||||
– |
10–15 |
Reserved |
Trip Status
The trip status register indicates the current status of the trip:
-
trip bit = 0: trip is not active.
-
trip bit = 1: trip is active.
The following table describes the values for each bit of the trip status register:
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Bit |
Description |
---|---|---|---|---|---|---|---|---|---|
0x270F |
10000 |
R |
– |
– |
INT16U |
– |
A/E |
– |
Trip status |
A/E |
0 |
Long-time protection Ir |
|||||||
A/E |
1 |
Short-time protection Isd |
|||||||
A/E |
2 |
Instantaneous protection Ii |
|||||||
A/E |
3 |
Ground-fault protection Ig |
|||||||
E |
4 |
Earth-leakage protection IΔn |
|||||||
A/E |
5 |
Integrated instantaneous protection |
|||||||
A/E |
6 |
Trip unit internal failure (STOP) |
|||||||
E |
7 |
Instantaneous with earth-leakage protection |
|||||||
A/E |
8 |
Unbalance motor protection Iunbal |
|||||||
A/E |
9 |
Jam motor protection Ijam |
|||||||
A/E |
10 |
Underload motor protection Iunderload |
|||||||
A/E |
11 |
Long-start motor protection Ilongstart |
|||||||
A/E |
12 |
Reflex tripping protection |
|||||||
– |
13–15 |
Reserved |