990-5998K-001

IP Capacity for UPS with Optional IP Kits

  • IP22 rating: UPS installed with IPX2 kit

  • IP30 rating: UPS installed with IP30 kit

  • IP32 rating: UPS installed with IP30 kit and IPX2 kit

  • IP40 rating: UPS installed with IP40 kit

  • IP42 rating: UPS installed with IP40 kit and IPX2 kit

See Hardware Options for IP kit overview.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.