990-66233A-001

Batteries

End of Discharge Voltage

This diagram is applicable for end of discharge (EOD) set as 1.6 V/cell at 3C – for VRLA only.

Standard VRLA Voltage Levels

NOTE: Specific configurations may differ from the general constraint shown above.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?