Airflow Values
Indicative Airflow Values in m3/Hour Based on a 30 °C Environment in Normal Operation Mode
UPS rating | 10 kVA | 15 kVA | 20 kVA | 30 kVA | 40 kVA |
---|---|---|---|---|---|
50% load |
83 |
83 |
94 |
243 |
276 |
70% load |
94 |
101 |
116 |
334 |
382 |
100% load |
130 |
150 |
157 |
408 |
456 |
Indicative Airflow Values in m3/Hour Based on a 40 °C Environment in Normal Operation Mode
UPS rating | 10 kVA | 15 kVA | 20 kVA | 30 kVA | 40 kVA |
---|---|---|---|---|---|
50% load |
130 |
150 |
157 |
408 |
456 |
70% load |
185 |
185 |
185 |
585 |
585 |
100% load |
185 |
185 |
185 |
585 |
585 |