990-66233A-001

Communication and Management

Modbus Modbus (RTU)
Output relays 3 x SELV configurable
Input contacts 3 x SELV configurable
Standard control panel 5 inch touchscreen display
Audible alarm Yes
Emergency power off (EPO)

Options:

  • Normally Closed (NC)

Internal switch

UIB
UOB
SSIB
MBB

Battery monitoring Available for external battery solutions
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?