990-66233A-001

Model List

UPS Models

  • Easy UPS 3S Pro 10 kVA 400 V 3:3 UPS for external batteries (E3SP10KH)

  • Easy UPS 3S Pro 15 kVA 400 V 3:3 UPS for external batteries (E3SP15KH)

  • Easy UPS 3S Pro 20 kVA 400 V 3:3 UPS for external batteries (E3SP20KH)

  • Easy UPS 3S Pro 30 kVA 400 V 3:3 UPS for external batteries (E3SP30KH)

  • Easy UPS 3S Pro 40 kVA 400 V 3:3 UPS for external batteries (E3SP40KH)

  • Easy UPS 3S Pro 15 kVA 400 V India 3:3 UPS for external batteries (E3SP15KHIN)

  • Easy UPS 3S Pro 20 kVA 400 V India 3:3 UPS for external batteries (E3SP20KHIN)

  • Easy UPS 3S Pro 30 kVA 400 V India 3:3 UPS for external batteries (E3SP30KHIN)

  • Easy UPS 3S Pro 40 kVA 400 V India 3:3 UPS for external batteries (E3SP40KHIN)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?