DOCA0248EN-18

New Features for Firmware Version 002.006.000

  • Security improvements in EcoStruxure Panel Server:

    • Security patch

      .
    • Firmware version 002.006.000 includes a security improvement (for more details, see issues fixed).

  • Panel Server allows you to configure an IPv6 address and an IPv6 gateway address.

    Setting

    Ethernet separated mode

    Ethernet switched mode

    Wi-Fi infrastructure

    ETH1 port

    ETH2 port

    IPv6 address associated to IPv6 prefix length setting.
    Used to configure a global or unique local address.

    Y

    Y

    Y

    Y

    IPv6 gateway address.
    Used to configure the IPv6 address of the gateway (usually a router) for communication with upstream systems.

    Y

    N

    Y

    Y

    Y: Setting available. The address can be generated automatically or set manually.
    N: Setting not available

    For more information about the settings, refer to chapters Ethernet Communication and Wi-Fi Infrastructure in DOCA0172•• EcoStruxure Panel Server - User Guide.

  • Panel Server supports new firmware versions of PowerLogic environmental sensors:

    • PowerLogic CL110 sensors with firmware version 2.1.5

    • PowerLogic TH110 sensors (ATMEL hardware) with firmware version 1.0.5

New Supported Devices

  • PowerLogic TH110 sensors (EFR32 hardware) with firmware version 2.0.0.

User Interface Improvements

  • In the Custom models webpage, the EPC Web access button allows you to access EPC Web tool directly to create custom device models.

  • In the Firmware update webpage, the Learn more button allows you to access information about Panel Server models and documentation on www.se.com.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.