DOCA0248EN-18

New Features for 002.002.000

  • Security improvements in Panel Server:

    • Password policy reinforced with new rules. Follow the new rules from your next password update. For more information about Password Requirements, refer to DOCA0172•• EcoStruxure Panel Server - User Guide.

    • Protect Plus: Install code introduced for discovery with heightened security of 16-character RF-ID wireless devices.

  • Wi-Fi access point allows you to use a PC to connect to the Wi-Fi network of the Panel Server, providing access to Panel Server webpages for device configuration, monitoring and firmware update.

  • Custom models can now include the Modbus discovery rules, which allows the Panel Server to use custom models in addition to built-in models to discover Modbus devices, without the need to use manual addition.

  • New supported devices: XB5R transmitters: ZBRT1 and ZBRT2. For more information about adding and removing ZBRT devices, refer to DOCA0172•• EcoStruxure Panel Server - User Guide.

  • Support for new measurements for motor controller devices:

    • Pole state

    • Contactor state

    • Speed setpoint

    • Motor speed

    • Direction of motor rotation

  • Introduction of maximum number of 50 custom models imported to Panel Server. Each model can have one current version and one available version.

User Interface Improvements

  • Monitoring & Control webpage:

    • Devices sorted by alphabetical usage in tree view. Devices with no usage assigned are displayed in a No usage category, at the end of the list. Each usage can be collapsed to improve clarity of display.

    • Width of first column is reduced in multi-device view to improve display.

    • A new data type Health state can be selected for display in multi-device view, with the following data:

      • Battery voltage

      • Internal temperature

      • RSSI link

  • Data management webpage: Devices are sorted by alphabetical usage in tree view. Devices with no usage assigned are displayed in a No usage category, at the end of the list. Each usage can be collapsed to improve clarity of display.

  • Trending webpage

    • In Device view, when more than one custom device is discovered using the same custom model, the device name is added to its associated measurement in the Data drop down list. This enables you to select the measurement associated with the device more easily.

    • In the Devices drop-down menu, devices are sorted by usage.

  • RF-ID of device is displayed in Settings > Wireless devices in the header for each wireless device

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.