DOCA0248EN-19

Major Fixes for Firmware Version 002.003.000

The following bugs are fixed in firmware version 002.003.000:

  • Instability experienced with connection to Wi-Fi infrastructure

  • Certain custom models created in EPC-Web tool after January 2025 were not compatible with Panel Server running firmware version 002.001.000. The import of the custom model was unsuccessful. For more information about compatibility, refer to the Custom Model Compatibility table in DOCA0172•• EcoStruxure Panel Server - User Guide.

  • For devices configured as Standard I/O and with I/O Contextualization set as Motor start, available values were On or Off and alarm was generated when the status passed from On to Off. From Panel Server firmware version 002.003.000, available values are Started and Not started, and alarm is generated when the status passes from Not started to Started. Historized data maintains the legacy terminology for data and events prior to update to firmware version 002.003.000, and new terminology for data and events after the update.

    NOTE: Check that your configuration takes into account this change to avoid spurious alarms.
  • When using the custom I/O contextualization of a Pulse counter device connected to the embedded input of the Panel Server, the format of the CSV files published through SFTP was not consistent with the format seen with firmware version 001.006.000. To see the data label IoCountMeasurement in CSV scripts, you needed to enter IoCountMeasurement in the Consumption meter element name field on the Panel Server web pages at Settings > Embedded input management.

    IMPORTANT: From Panel Server firmware version 002.001.000, the csv file displays Measurement.IoCountMeasurement as a column header data label for the parameter IoCountMeasurement. Remap ETL applications to take account of this difference.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.