DOCA0248EN-18

New Features for 002.000.000

  • Increase in the maximum number of alarms that can be selected for publication from 100 to 500. Among the 500 alarms, a maximum of 300 can be from Modbus-SL devices.

  • Addition of the following supported devices:

    • Wireless devices:

      • Exiway Light device

      • MasterPacT MTZ with MicroLogic Active AP or EP

    • Modbus devices: BSCM Modbus SL/ULP module

  • Wi-Fi access point enables you to connect to the Wi-Fi network of the Panel Server from a smartphone running the Schneider Electric EcoStruxure Power Commission mobile app . From the app you can configure connected devices.

  • Addition of local time zone which can be set at Settings > General > Date and time. When set, the local time zone is used:

    • For data displayed on the following webpages:

      • Monitoring & Control

      • Home

      • Trending

    • In emails for alarms

    • For data published to an SFTP or HTTPS server

    • For data exported in a local file

    UTC is used to publish to cloud applications and for logging data, even when local time zone is set.

  • Addition of support for RSTP protocol allowing robust Ethernet ring topologies for critical applications. RSTP is available only when the Panel Server is configured in switched mode.

  • Addition of the following supported measurements:

    • Steam volume (m3)

    • Steam flow (m3/s)

    • Steam mass flow (kg/s)

    • Air volume (m3)

    • Air flow (m3/s)

    These measurements are specified in a custom device model created in the EcoStruxure Power Commission web portal tool and imported into the Panel Server. The measurement values are available in the Monitoring & Control webpage.

  • Panel Server webpage user experience improvements:

    • Loading time of webpages improved.

    • Data management page improvements:

      • In Local export, addition of the choice of a single device or All devices when the period selection is made.

      • A banner message gives information about the purpose and result of selecting measurements and alarms.

      • Date and time of last measurement data update is displayed at the top of the page.

    • In Monitoring & Control webpage, addition of date and time of last measurement data update at the top of the page.

    • In Maintenance > Firmware update page, addition of following sections:

      • Retrieve the correct firmware with button to click to allow you to download the correct firmware update for your Panel Server directly to your PC.

      • Further information with button to click to allow you to access general information related to Panel Server products.

    • Home page has improved loading time.

    • Trending page has the following improvements:

      • Granularity (display data by hour, day or month) added in compare function.

      • Custom period added in Device view and Aggregated view.

      • Editable start time of trending period added in addition to date.

      • Graphical indication (shading in bar charts, orange dot in line graphs) and tooltip added to indicate data points that are calculated by extrapolation or that data points may be missing due to modified sampling period.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.