DOCA0248EN-19

General Features

The following table presents the availability of general features on Panel Server Advanced in firmware version 002.006.001.

Available

Not available

General features

Availability

Functionality

Separated network topology

Switched network topology

Connection to Edge Control (EcoStruxure Power Monitoring Expert, EcoStruxure Power Operation,EcoStruxure Building Operation, any Building Management System, or third-party monitoring or supervision system)

Ability to disable concurrently and permanently the wireless networks (Wi-Fi and IEEE 802.15.4) by using Panel Server webpages

Wi-Fi

2.4 GHz

5 GHz

External Wi-Fi antenna (reference: PASA-ANT1)

Wi-Fi access point, available to connect a smartphone running the Schneider Electric EcoStruxure Power Commission mobile app

Human Machine Interface (HMI)

FDM128 Ethernet display

Configuration

User management by single user account

User management by multiple users with Role-Based Access Control (RBAC)

Alarms

  • In general, publication of alarms supported by the end devices.

  • Publication of alarms related to the following:

    • Communication issue between a device and Panel Server when available from the end devices

    • Alarm associated to ERMS on circuit breaker

    • The three levels of alarms from HeatTag sensors

    • Alarms associated to Breaker I/O device connected downstream to an I/O Smart Link gateway

    • Communication loss alarm for wireless device connected downstream to a child gateway.

Protocols

IEEE 802.15.4

Modbus TCP/IP server

Modbus TCP/IP client

DHCP client

DHCP server

DPWS server

HTTPS

SFTP client

RSTP

Data export

Panel Server webpages for publication on SFTP server or HTTPS server

Publication on Schneider Electric cloud by using Panel Server webpages

CSV export on PC by using Panel Server webpages

Maximum Configuration

The maximum number of devices that can be configured in a system with a Panel Server Advanced depends on the type of connected devices:

Device type

Maximum number of concurrent devices

Wireless device (not supported by PAS600LWD and PAS600PWD)

PowerTag Energy sensors

85

PowerLogic Tag energy sensors

85

Acti9 Active devices

85

Wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers

85

MasterPacT MTZ circuit breakers with MicroLogic Active AP or EP control unit

8

Wireless CO2 sensors

100

Wireless temperature and humidity sensors

100

PowerTag Ambient sensors

100

PowerLogic TH110/CL110 environmental sensors

100

PowerLogic Thermal Tag TH150/TH200 wireless temperature sensors

100

PowerLogic HeatTag sensors

15

PowerTag Control devices

10

PowerLogic PD100 devices

15

Exiway Link devices

20

XB5R transmitters (ZBRT)

100

The recommendation for a mixed configuration of wireless devices is as follows:

  • Any combination of wireless devices listed in the rows above should not exceed 40 devices.

  • The total number of PowerTag Control, PowerLogic HeatTag, PowerLogic PD100, MicroLogic Active AP or EP control unit for MasterPacT MTZ, and Exiway Link devices should not exceed 20 devices.

Modbus-SL devices

Modbus-SL devices other than I/O devices:

32

NOTE: The maximum number depends on the serial line length and the type of device(s).

I/O devices:

  • I/O Smart Link device

  • Acti9 Smartlink Modbus-SL device

  • SmartLink SIB gateway

  • 8 I/O Smart Link or Acti9 Smartlink Modbus-SL devices connected to Panel Server serial line

  • OR

    1 SmartLink SIB + 7 I/O Smart Link or Acti9 Smartlink Modbus-SL devices

  • OR

    8 SmartLink SIB

Modbus TCP/IP devices

Devices physically connected to the Panel Server and virtual devices, that is, IEEE 802.15.4 wireless devices connected to a child Panel Server gateway.

128

NOTE: The Panel Server supports 64 simultaneous Modbus TCP/IP client connections (for example, SCADA system).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.