DOCA0248EN-19

Panel Server Advanced Gateway

Panel Server Advanced is a high performance, all-in-one gateway used to retrieve data from IEEE 802.15.4 and Modbus devices.

Panel Server Advanced is a data concentrator for wireless devices (see detailed list).

Panel Server Advanced is available with different power supplies:

  • PAS800: 110–277 Vac/Vdc

  • PAS800L : 24 Vdc

  • PAS800P : Power over Ethernet (PoE)

Panel Server Advanced offers the following features:

  • Two 10/100BASE-T Ethernet RJ45 ports

  • Upstream Modbus TCP/IP connectivity (edge connection)

  • Upstream Wi-Fi connectivity

  • Wi-Fi access point

  • Downstream Modbus TCP/IP connectivity

  • Downstream IEEE 802.15.4 connectivity

  • Downstream Modbus-SL connectivity

  • Two digital inputs (PAS800L)

  • Wi-Fi external antenna

  • IEEE 802.15.4 external antenna

  • Data sampling

  • Data logging (3 years)

  • Compatible with the following commissioning tools of Panel Server and connected devices:

    • EcoStruxure Power Commission software

    • EcoStruxure Panel Server webpages

  • Compatible with the following Schneider Electric cloud applications:

    • EcoStruxure Energy Hub

    • EcoStruxure Asset Advisor

    • EcoStruxure Resource Advisor

Convention

EcoStruxure Panel Server is hereafter referred to as Panel Server.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.