DOCA0248EN-19

Modbus TCP/IP Devices

The following table shows the minimum Panel Server Advanced firmware version required to enable Ethernet communication with devices for real-time measurement monitoring in Panel Server webpages.

Device family

Device

Minimum Panel Server Advanced firmware version

Power meter

PowerLogic CM3250 circuit monitor

001.003.002

Power meter

PowerLogic CM3350 circuit monitor

001.003.002

Power meter

PowerLogic CM4000 circuit monitor

001.003.002

Power meter

PowerLogic EM3570 energy meter

METSEEM3570

002.005.000

Power meter

PowerLogic EM3570A energy meter

METSEEM3570A

002.005.000

Power meter

PowerLogic EM3570X energy meter

METSEEM3570X

002.005.000

Power meter

PowerLogic EM3570AX energy meter

METSEEM3570AX

002.005.000

Power meter

PowerLogic PM5320 power meter

METSEPM5320

001.003.002

Power meter

PowerLogic PM5340 power meter

METSEPM5340

001.003.002

Power meter

PowerLogic PM5341 power meter

METSEPM5341

001.003.002

Power meter

PowerLogic PM5560 power meter

METSEPM5560

001.003.002

Power meter

PowerLogic PM5561 power meter

METSEPM5561

001.003.002

Power meter

PowerLogic PM5563 power meter

METSEPM5563

001.003.002

Power meter

PowerLogic PM5570 power meter

METSEPM5570

001.003.002

Power meter

PowerLogic PM5580 power meter

METSEPM5580

001.003.002

Power meter

PowerLogic PM5650 power meter

METSEPM5650

001.003.002

Power meter

PowerLogic PM5660 power meter

METSEPM5660

001.003.002

Power meter

PowerLogic PM5661 power meter

METSEPM5661

001.003.002

Power meter

PowerLogic PM5760 power meter

METSEPM5760

001.003.002

Power meter

PowerLogic PM5761 power meter

METSEPM5761

001.003.002

Power meter

PowerLogic PM810 power meter

001.003.002

Power meter

PowerLogic PM820 power meter

001.003.002

Power meter

PowerLogic PM850 power meter

001.003.002

Power meter

PowerLogic PM870 power meter

001.003.002

Power meter

PowerLogic PM8000 power meter

METSEPM8210

001.003.002

METSEPM8213

001.003.002

METSEPM8214

001.003.002

METSEPM8240

001.003.002

METSEPM8243

001.003.002

METSEPM8244

001.003.002

METSEPM82101

001.003.002

METSEPM82103

001.003.002

METSEPM82104

001.003.002

METSEPM82143

001.003.002

METSEPM82144

001.003.002

METSEPM82401

001.003.002

METSEPM82403

001.003.002

METSEPM82404

001.003.002

METSEPM82443

001.003.002

METSEPM82444

001.003.002

Transformer monitoring

NT935 ETH

001.003.002

Circuit Breakers and Associated Trip Units

The following table shows the circuit breaker devices supported by Panel Server Advanced for real-time measurement monitoring in Panel Server webpages.

NOTE: Update associated IFE and EIFE interfaces to firmware version 003.009.010 or later to ensure that measurements are displayed and published correctly in the Panel Server.

The circuit breaker devices and associated trip units are connected to Panel Server through one of the interfaces indicated in the table below.

  • Y: the device is supported by Panel Server.
  • N: the device is not yet supported by Panel Server using a pre-defined model. Use a custom model to connect to this device.
  • N/A: not applicable

Circuit breaker

Trip unit

Connected to
IFE Ethernet interface IFE Ethernet switchboard server EIFE embedded Ethernet interface
LV434010 LV434001 LV434011 LV434002 LV851001
MasterPacT MTZ

MicroLogic 2.0 X

Y

Y

Y

Y

Y

MicroLogic 3.0 X

N

N

N

N

Y

MicroLogic 5.0 X

N

N

N

N

Y

MicroLogic 6.0 X

Y

Y

Y

Y

Y

MicroLogic 7.0 X

N

N

N

N

Y

MicroLogic 5.0 Xi

Y

Y

Y

Y

Y

MasterPacT NT/NW

MicroLogic 2.0 A

Y

Y

Y

Y

N/A

MicroLogic 3.0 A

Y

Y

Y

Y

N/A

MicroLogic 5.0 A

Y

Y

Y

Y

N/A

MicroLogic 6.0 A

Y

Y

Y

Y

N/A

MicroLogic 7.0 A

Y

Y

Y

Y

N/A

MicroLogic 2.0 E

Y

Y

Y

Y

N/A

MicroLogic 5.0 E

Y

Y

Y

Y

N/A

MicroLogic 6.0 E

Y

Y

Y

Y

N/A

MicroLogic 5.0 P

Y

Y

Y

Y

N/A

MicroLogic 6.0 P

Y

Y

Y

Y

N/A

ComPacT NS

MicroLogic 7.0 A

N

N

N

N

N/A

MicroLogic 7.0 H

Y

Y

Y

Y

N/A

ComPacT NSX

MicroLogic 5.2 A

Y

Y

Y

Y

N/A

MicroLogic 6.2 A

Y

Y

Y

Y

N/A

MicroLogic 5.2 E

Y

Y

Y

Y

N/A

MicroLogic 6.2 E

Y

Y

Y

Y

N/A

MicroLogic 7.2 E

Y

Y

Y

Y

N/A

MicroLogic 5.3 E

Y

Y

Y

Y

N/A

MicroLogic 6.3 E

Y

Y

Y

Y

N/A

MicroLogic 7.3 E

Y

Y

Y

Y

N/A

PowerPacT H-, J-, and L-frame

MicroLogic 5.3 A

Y

Y

Y

Y

N/A

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.