DOCA0248EN-19

New Features for Version 002.001.000

  • Support for the following commands from cloud to Exiway Link devices

    • Locate an Exiway Link device to make it blink for five minutes

    • Disable or enable periodic tests

    • Start functional test

    • Switch light on or off

    • Synchronize Exiway Link devices

  • Addition of the following commands from webpages to Exiway Link devices:

    • Locate an Exiway Link device to make it blink for five minutes

    • Disable or enable periodic tests

    • Start functional test

  • Addition of sampling and publication of following real-time environmental measurements, depending on device connected:

    • Battery voltage

    • Internal temperature

    • RSSI link

  • Addition of export of data selected and displayed on Trending page

Panel Server webpage user experience improvements:

  • Monitoring and Control page organized with two views:

    • Device view: device-centric view allows you to display data for one device. Data is displayed as widgets for each data type.

    • Multi-device view: select up to 5 devices and 2 data types to display. The selection is maintained when clicking away and returning. A link on each device name displays the device view directly.

  • Addition of alarm severity in Data management page for individual devices.

  • Wireless device connection status indicator: added connection status in orange for reduced connection quality with possible loss of communication.

  • Link from Notifications page to Monitoring & Control page for individual device to see details of alarm.

  • In Publication settings, addition of Include past data toggle switch to allow the choice of including all past date (up to three months) in first publication.

  • In Trending pages, display data by selecting from the following options:

    • Individual usages: one or several

    • Main usages: six main usages by consumption

    • All usages: exhaustive list of data

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.