DOCA0248EN-19

Modbus Serial Devices

The following table shows the minimum Panel Server Advanced firmware version required to enable Modbus communication with devices for real-time measurement monitoring in Panel Server webpages.

For third-party devices not listed in the table, data of the device can be accessed by reading the different Modbus registers. All data available from the Modbus registers will not be accessible and displayed in the Panel Server webpages.

Device family

Device

Minimum Panel Server Advanced firmware version

Power meter

PowerLogic CM3250 circuit monitor

001.003.002

Power meter

PowerLogic CM3350 circuit monitor

001.003.002

Power meter

PowerLogic CM4000 circuit monitor

001.003.002

Power meter

PowerLogic EM3550 energy meter

001.003.002

Power meter

PowerLogic EM3550A energy meter

001.003.002

Power meter

PowerLogic EM3555 power and energy meter

001.003.002

Power meter

PowerLogic EM3555A energy meter

001.003.002

Power meter

PowerLogic EM4200 Enercept power and energy meter

001.003.002

Power meter

PowerLogic EM6400NG energy meter

METSEEM6400NGRSCL2

001.003.002

Power meter

METSEEM6400NGRSCL5

001.003.002

Power meter

METSEEM6400NGRSCL1

001.003.002

Power meter

PowerLogic EM6433H energy meter

METSEEM6433HCL10RS

001.003.002

Power meter

METSEEM6433HCL05RS

001.003.002

Power meter

PowerLogic EM6436H energy meter

METSEEM6436HCL10RS

001.003.002

Power meter

METSEEM6436HCL05RS

001.003.002

Power meter

PowerLogic EM7200 power and energy

30002055

001.003.002

30002198

001.003.002

30002975

001.003.002

Power meter

EM3100 energy meter

METSEEM3122

002.003.000

EM3200 energy meter

METSEEM3224

002.003.000

EM3300 energy meter

METSEEM3322

002.003.000

EM3400 energy meter

METSEEM3424

002.003.000

EM3700 energy meter

METSEEM3724

002.003.000

Power meter

EasyLogic PM1130H meter

METSEPM1130HCL05RS

001.003.002

Power meter

METSEPM1130HCL05RD

001.003.002

Power meter

EasyLogic PM2130 meter

METSEPM2130D

001.003.002

Power meter

EasyLogic PM2220 meter

METSEPM2220D

001.003.002

Power meter

EasyLogic PM2220 meter

METSEPM2220

001.003.002

Power meter

EasyLogic PM2230 meter

METSEPM2230D

001.003.002

Power meter

EasyLogic PM2230 meter

METSEPM2230

001.003.002

Power meter

Acti9 iEM2050 energy meter

A9MEM2050

001.003.002

Power meter

Acti9 iEM2055 energy meter

A9MEM2055

001.003.002

Power meter

Acti9 iEM2150 energy meter

A9MEM2150

001.003.002

Power meter

Acti9 iEM2155 energy meter

A9MEM2155

001.003.002

Power meter

Acti9 iEM2155 energy meter

A9MEM2155

001.003.002

Power meter

Acti9 iEM2155 energy meter

A9MEM2155

001.003.002

Power meter

Acti9 iEM2455 energy meter

A9MEM2455

001.003.002

Power meter

Acti9 iEM3150 energy meter

A9MEM3150

001.003.002

Power meter

Acti9 iEM3155 energy meter

A9MEM3155

001.003.002

Power meter

Acti9 iEM3250 energy meter

A9MEM3250

001.003.002

Power meter

Acti9 iEM3255 energy meter

A9MEM3255

001.003.002

Power meter

Acti9 iEM3350 energy meter

A9MEM3350

001.003.002

Power meter

Acti9 iEM3355 energy meter

A9MEM3355

001.003.002

Power meter

Acti9 iEM3455 energy meter

A9MEM3455

001.003.002

Power meter

Acti9 iEM3555 energy meter

A9MEM3555

001.003.002

Power meter

PowerLogic PM3250 power meter

001.003.002

Power meter

PowerLogic PM3255 power meter

001.003.002

Power meter

PowerLogic PM5110 power meter

001.003.002

Power meter

PowerLogic PM5111 power meter

001.003.002

Power meter

PowerLogic PM5310 power meter

001.003.002

Power meter

PowerLogic PM5330 power meter

001.003.002

Power meter

PowerLogic PM5331 power meter

001.003.002

Power meter

PowerLogic PM5560 power meter

001.003.002

Power meter

PowerLogic PM5561 power meter

001.003.002

Power meter

PowerLogic PM5563 power meter

001.003.002

Power meter

PowerLogic PM5570 power meter

METSEPM5570

001.003.002

Power meter

PowerLogic PM5580 power meter

METSEPM5580

001.003.002

Power meter

PowerLogic PM5650 power meter

METSEPM5650

001.003.002

Power meter

PowerLogic PM5660 power meter

METSEPM5660

001.003.002

Power meter

PowerLogic PM5661 power meter

METSEPM5661

001.003.002

Power meter

PowerLogic PM5760 power meter

METSEPM5760

001.003.002

Power meter

PowerLogic PM5761 power meter

METSEPM5761

001.003.002

Power meter

PowerLogic PM810 power meter

001.003.002

Power meter

PowerLogic PM820 power meter

001.003.002

Power meter

PowerLogic PM850 power meter

001.003.002

Power meter

PowerLogic PM870 power meter

001.003.002

Power meter

PowerLogic PM8000 power meter

001.003.002

I/O module

Acti 9 Smartlink Modbus

A9XMSB11
with FW v001.003.007

001.003.002

I/O module

I/O Smart Link

A9XMSB11
with FW v003.00X.00Y

001.007.000

I/O module

Acti 9 Smartlink SI B

A9XMZA08

001.003.002

Protection relay

Easergy Sepam Series 20 BSTM protection relay

001.003.002

Protection relay

Easergy Sepam Series 40 protection relay

001.003.002

Transformer monitoring

NT935

001.003.002

Passive power correction

PowerLogic power factor controller VarPlus Logic VL6

001.004.000

Passive power correction

PowerLogic power factor controller VarPlus Logic VL12

001.004.000

Insulation monitoring

Vigilohm IM20 insulation monitoring device*

IMD-IM20

001.005.001

Insulation monitoring

Vigilohm IM20H insulation monitoring device*

IMD-IM20–H

001.005.001

Insulation monitoring

Vigilohm IM400 insulation monitoring device*

IMD-IM400

001.005.001

Insulation monitoring

Vigilohm IM400C insulation monitoring device*

IMD-IM400C

001.005.001

Insulation monitoring

Vigilohm IM400L insulation monitoring device*

IMDIM400L

001.005.001

Insulation monitoring

Vigilohm IM400N insulation monitoring device*

IMDIM400N

001.005.001

Insulation monitoring

Vigilohm IM400LTHR insulation monitoring device*

IMDIM400LTHR

001.005.001

Insulation monitoring

Vigilohm IM400THR insulation monitoring device*

IMDIM400THR

001.005.001

Insulation monitoring

Vigilohm IM400THRN insulation monitoring device*

IMDIM400THRN

001.005.001

Insulation monitoring

Vigilohm IMDIFL12MCT insulation fault locator*

001.005.001

Circuit Breakers and Associated Trip Units

The following table shows the Modbus-SL circuit breaker devices supported by Panel Server Advanced for real-time measurement monitoring in Panel Server webpages.

NOTE: Update associated IFM interface LV434000 to firmware version 003.001.010 or later to ensure that measurements are displayed and published correctly in the Panel Server.

The circuit breaker devices and associated trip units are connected to Panel Server through the interface or module indicated in the table below.

  • Y: the device is supported by Panel Server
  • N: the device is not yet supported by Panel Server using a pre-defined model. Use a custom model to connect to this device.
  • N/A: not applicable

Circuit breaker

Trip unit

Connected to

IFM Modbus-SL interface BSCM Modbus SL/ULP Module
TVR00210 LV434000

LV434220

MasterPacT MTZ

MicroLogic 2.0 X

N/A

Y

N/A

MicroLogic 3.0 X

N/A

Y

N/A

MicroLogic 5.0 X

N/A

Y

N/A

MicroLogic 6.0 X

N/A

Y

N/A

MicroLogic 7.0 X

N/A

Y

N/A

MicroLogic 5.0 Xi

N/A

N

N/A

MasterPacT NT/NW

MicroLogic 2.0 A

N

N

N/A

MicroLogic 3.0 A

N

N

N/A

MicroLogic 5.0 A

N

N

N/A

MicroLogic 6.0 A

N

N

N/A

MicroLogic 7.0 A

Y

Y

N/A

MicroLogic 2.0 E

N

N

N/A

MicroLogic 5.0 E

N

N

N/A

MicroLogic 6.0 E

N

N

N/A

MicroLogic 5.0 P

Y

Y

N/A

MicroLogic 6.0 P

Y

Y

N/A

ComPacT NS

MicroLogic 7.0 A

Y

Y

N/A

MicroLogic 7.0 H

N

N

N/A

ComPacT NSX

MicroLogic 5.2 A

N

N

Y

MicroLogic 6.2 A

Y

Y

Y

MicroLogic 5.2 E

Y

Y

Y

MicroLogic 6.2 E

Y

Y

Y

MicroLogic 7.2 E

Y

Y

Y

MicroLogic 5.3 E

Y

Y

Y

MicroLogic 6.3 E

N

N

Y

MicroLogic 7.3 E

Y

Y

Y

PowerPacT H-, J-, and L-frame

MicroLogic 5.2 A

N

N

Y

MicroLogic 5.3 A

N

N

Y

MicroLogic 6.2 A

N

N

Y

MicroLogic 5.2 E

N

N

Y

MicroLogic 6.2 E

N

N

Y

MicroLogic 7.2 E

N

N

Y

MicroLogic 5.3 E

N

N

Y

MicroLogic 6.3 E

N

N

Y

MicroLogic 7.3 E

N

N

Y

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.