General Features
The following table presents the availability of general features on Panel Server Advanced in firmware version 002.000.000.
General features |
Availability |
||
---|---|---|---|
Functionality |
Separated network topology |
● |
|
Switched network topology |
● |
||
Connection to Edge Control (EcoStruxure Power Monitoring Expert, EcoStruxure Power Operation,EcoStruxure Building Operation, any Building Management System, or third-party monitoring or supervision system) |
● |
||
Ability to disable concurrently and permanently the wireless networks (Wi-Fi and IEEE 802.15.4) by using Panel Server webpages |
● |
||
Wi-Fi |
2.4 GHz |
● |
|
5 GHz |
● |
||
External Wi-Fi antenna (reference: PASA-ANT1) |
● |
||
Wi-Fi access point, available to connect a smartphone running the Schneider Electric EcoStruxure Power Commission mobile app |
● |
||
IEEE 802.15.4 communication |
Wireless device |
Maximum concurrent number of devices |
● |
PowerTag Energy sensors |
85 |
||
PowerLogic Tag energy sensors |
85 |
||
Acti9 Active devices |
85 |
||
Wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers |
85 |
||
MasterPacT MTZ circuit breakers with MicroLogic Active AP or EP control unit |
8 |
||
Wireless CO2 sensors |
100 |
||
Wireless temperature and humidity sensors |
100 |
||
PowerTag A devices |
100 |
||
PowerTag Ambient sensors |
100 |
||
Easergy TH110/CL110 environmental sensors |
100 |
||
PowerLogic HeatTag sensors |
15 |
||
PowerTag Control devices |
10 |
||
PowerLogic PD100 devices |
15 |
||
Exiway Light devices |
10 |
||
The recommendation for a mixed configuration is as follows:
|
|||
Modbus TCP/IP communication |
128 Modbus TCP/IP devices maximum including devices physically connected to the Panel Server and virtual devices (that is, IEEE 802.15.4 devices connected to a child Panel Server gateway) NOTE: The Panel Server supports 64 simultaneous Modbus TCP/IP client connections (for
example, SCADA system).
|
● |
|
Modbus SL communication |
32 Modbus SL devices maximum |
● |
|
Human Machine Interface (HMI) |
FDM128 Ethernet display |
● |
|
Configuration |
User management by single user account |
● |
|
User management by multiple users with Role-Based Access Control (RBAC) |
● |
||
Alarms |
|
● |
|
Protocols |
Modbus TCP/IP server |
● |
|
Modbus TCP/IP client |
● |
||
DHCP client |
● |
||
DHCP server |
● |
||
DPWS server |
● |
||
HTTPS |
● |
||
SFTP client |
● |
||
RSTP |
● |
Data export |
Panel Server webpages for publication on SFTP server or HTTPS server |
● |
Publication on Schneider Electric cloud by using Panel Server webpages |
● |
|
CSV export on PC by using Panel Server webpages |
● |