DUG_ELKO - Smart ZB Thermostat 16 A_WH-00

Setting boost mode manually

You can enable and disable boost mode manually.
When enabled the temperature increases by 2° C for temperature control modes (P1 to P8) and by +2 for regulator mode (P9) over the current temperature.

To enable boost mode:

  1. Press O button once to enter boost menu.


    +1 flashes on thermostat matrix.
  2. Use +/- button to navigate between the boost hours from +1 to +3.

    After selecting the boost hours, thermostat will save and exit boost mode if there is no interaction within 5 s.

For example:
If the ambient temperature is 20° C and the set point is 18° C, there is no heat demand. If you want to increase the set point temperature for a short while you can boost heating. When boosted, the set point becomes 22° C (20 +2) for the desired boost duration. Once that duration ends, the set point goes back to its initial value, 18° C, or to the scheduled value if scheduling is enabled.


To disable boost mode:

  1. Press O button once.
    +1 flashes on thermostat matrix.

  2. Press + button for thermostat to display – – (boost cancel).

    After selecting the boost cancel, thermostat will save and exit boost mode if there is no interaction within 5 s.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?