DUG_ELKO - Smart ZB Thermostat 16 A_WH-00

Turning on/off the device manually

When thermostat is not in use, you can turn on/off the device manually
NOTE: Make sure to disable childlock before turning off the device.

Press for > 10 s to turn off.

When thermostat is fully off:

  • LED displays no room temperature

  • Does not control room temperature

  • Outputs remain off

  • On initial interaction, the device shows an “X” on the display to show that it is off.

Wake the thermostat by pressing /O/+ once, thermostat matrix display X and then press /O/+ button for > 5 s to turn.

When the thermostat is turned on, it returns to its last state.

NOTE: When the thermostat is turned on/off manually, its status is not displayed in the ELKO Smart app.
IMPORTANT: If your thermostat is OFF, your home is not protected against frost. Using the current version of the ELKO Smart app, you can not switch back a thermostat ON. It can only be turned ON manually.
Hence, if you leave for holidays, it is recommended to lower the set point to the minimum, in frost protection level, instead of turning the thermostat OFF.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?