990-91380L-001

Connect the External Communication Cables

  1. Connect the external communication cables to the ports in the system level controller.
    1. Universal I/O port for built-in network management card.

    2. Modbus port for built-in network management card.

    3. Network port for built-in network management card. Use a shielded network cable.

    NOTE: Check that you are connecting to the correct port to avoid network communication conflicts.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.