990-91380L-001

IEC-Specific Specifications

Surge Protection Device (SPD)

DANGER
Hazard of electric shock, explosion, or arc flash
This UPS is OVCII (Over Voltage Category Class II) compliant. This UPS must only be installed in an OVCII compliant environment.
  • If the UPS is installed in an environment with an OVC rating higher than II, an SPD (surge protection device) must be installed upstream of the UPS to reduce the overvoltage category to OVCII.
  • The SPD must include a status indicator to show the user if the SPD is operational or is no longer functioning according to design. The status indicator may be visual and/or audible and/or may have remote signalling and/or output contact capability in accordance with IEC 62040-1.
Failure to follow these instructions will result in death or serious injury.

Surge Protection Device Requirements

Select a surge protection device that complies with the following requirements:

Class Type 2
Rated voltage (Ur) 230/400 V, 277/480 V
Voltage protection level (Up) < 2.5 kV
Short circuit rating (Isccr)* According to installation prospective short circuit level
Earthing system* TN-S, TT, IT, TN-C
Poles 3P/4P depending on earthing configuration
Standards IEC 61643-11 / UL 1449
Monitoring Yes

Upstream and Downstream Protection for IEC

NOTE: For local directives which require 4-pole circuit breakers: If neutral conductor is expected to carry a high current, due to line-neutral non-linear load, the circuit breaker must be rated according to expected neutral current.

The bypass/output breakers are sized based on the nominal current +10%. This is to accommodate either low grid voltage or deviation in length between parallel UPSs. The battery breakers are sized based on end-of-discharge voltage which has been defined as 380 VDC.

Preconditions for Live Swap of Power Modules

Live Swap of power modules is only allowed under the following preconditions for the UPS installation; Follow either scenario 1 or scenario 2:

Preconditions for UPS installation – scenario 1 with instantaneous override values and trip times set according to the tables below in Recommended Upstream Protection for IEC Preconditions for UPS installation – scenario 2 with alternative breaker configurations supported with GVLOPT011 and breaker with ERMS mode*
Circuit breakers must have instantaneous trip time of maximum 60 ms. Circuit breakers must be installed for input (unit input breaker UIB) and bypass (static switch input breaker SSIB).
Circuit breakers must have instantaneous override values set according to the table below. Circuit breakers (UIB, SSIB) must be equipped with NEC 240.87, NFPA70E, IEEE1584, or EN51110-1 compliant ERMS mode.
Circuit breakers must be installed for input (unit input breaker UIB) and bypass (static switch input breaker SSIB). For parallel systems with three or more UPSs: Circuit breakers must be installed for the output (unit output breaker UOB) of each UPS. The unit output breaker (UOB) is sized as the static switch input breaker (SSIB).
For parallel system with three or more UPSs: Circuit breakers must be installed for the output (unit output breaker UOB) of each UPS. The unit output breaker (UOB) is sized as the static switch input breaker (SSIB). Circuit breaker (UOB) must be equipped with NEC 240.87, NFPA70E, IEEE1584, or EN51110-1 compliant ERMS mode.
Live Swap is not supported for >65kAbf installations where current limiting disconnect devices are used to protect the UPS. GVLOPT011 (Galaxy VL door switch kit) must be installed in the UPS and connected so ERMS mode is set to ON on UIB and SSIB and UOB when the front door of the UPS is opened.
  In ERMS mode, the instantaneous trip current shall be set to 5000 A or less. All time-delay settings shall be set to zero.

Schneider Electric reserves the right to remove the Live Swap label from the product front if the preconditions for scenario 1 or scenario 2 are not met.

DANGER
Hazard of electric shock, explosion, or arc flash
Only perform Live Swap of the power modules in UPS installations that follow the preconditions for scenario 1 or scenario 2.
Failure to follow these instructions will result in death or serious injury.

Upstream Protection for IEC and Minimum Prospective Phase-To-Earth Short Circuit at the UPS Input/Bypass Terminals

DANGER
Hazard of electric shock, explosion, or arc flash
The upstream overcurrent protective device (and its settings) must be sized to ensure a disconnecting time within 0.2 seconds in case of a short circuit between the input/bypass phase and the UPS enclosure.
Failure to follow these instructions will result in death or serious injury.
Compliance is assured with the recommended breaker (and its settings) from the table below.

Recommended Upstream Protection for IEC

IkPh-PE is the minimum prospective phase-to-earth short circuit current required at the input/bypass terminals of the UPS. The IkPh-PE in the table is based on the recommended protective device.

UPS rating 200 kW
  Input Bypass/Output Battery
IkPh-PE (kA) 5 4.5 NA
Voltage (V) 380 400 415 440 380 400 415 440 380-440
Breaker type
Breaker type

ComPacT NSX 400H MicroLogic 2.0 (3P: C4032D400, 4P: C4042D400)

ComPacT NS 630S DC TM-D (C634TM630D)
In/trip unit 400 400 400 400 400 400 400 400 360
Io 400 400 360 360 360 360 320 320
Ir setting 0.93 0.92 0.98 0.93 0.95 0.9 0.98 0.93 0.9
Ir 372 368 353 335 342 324 314 298 567
Isd <10 x Ir <10 x Ir <10 x Ir <10 x Ir 10 x Ir 10 x Ir 10 x Ir 10 x Ir <10 x Ir
UPS rating 250 kW
  Input Bypass/Output Battery
IkPh-PE (kA) 6 6 NA
Voltage (V) 380 400 415 440 380 400 415 440 380-440
Breaker type
Breaker type
ComPacT NSX 630H MicroLogic 2.0 (3P: C6332D630, 4P: C6342D630) ComPacT NSX 400H MicroLogic 2.0
(3P: C4032D400, 4P: C4042D400)
MasterPacT NW10HDC-D MicroLogic 1.0 DC (48649+65272)
In/trip unit 630 630 630 630 630 630 400 400 1000
Io 500 500 450 450 450 450 400 400
Ir setting 0.93 0.92 0.98 0.93 0.95 0.9 0.98 0.93
Ir 465 460 441 418 428 405 392 372 1000
Isd <10 x Ir <10 x Ir <10 x Ir <10 x Ir 10 x Ir 10 x Ir 10 x Ir 10 x Ir 1500
UPS rating 300 kW
  Input Bypass/Output Battery
IkPh-PE (kA) 7.5 7 NA
Voltage (V) 380 400 415 440 380 400 415 440 380-440
Breaker type
Breaker type
ComPacT NSX 630H MicroLogic 2.0 (3P: C6332D630, 4P: C6342D630) MasterPacT NW10HDC-D MicroLogic 1.0 DC (48649+65272)
In/trip unit 630 630 630 630 630 630 630 630 1000
Io 570 570 570 500 570 500 500 450
Ir setting 0.98 0.97 0.93 1 0.9 0.98 0.94 1
Ir 559 553 530 500 513 490 470 450 1000
Isd <10 x Ir <10 x Ir <10 x Ir <10 x Ir 10 x Ir 10 x Ir 10 x Ir 10 x Ir <10 x Ir
UPS rating 350 kW
  Input Bypass/Output Battery
IkPh-PE (kA) 8.5 8 NA
Voltage (V) 380 400 415 440 380 400 415 440 380-440
Breaker type
Breaker type
ComPacT NS800H MicroLogic 5.0 (3P: 33553, 4P: 33556) ComPacT NSX 630H MicroLogic 2.0 (3P: C6332D630, 4P: C6342D630) MasterPacT NW10HDC-D MicroLogic 1.0 DC (48649+65272)
In/trip unit 800 800 630 630 630 630 630 630 1000
Io 630 630 630 630 570 570 570
Ir setting 0.9 0.8 0.98 0.93 0.95 1 0.96 0.92
Ir 720 640 617 586 598 570 547 524 1000
Isd/ii* <10 x Ir <10 x Ir <10 x Ir <10 x Ir 10 x Ir 10 x Ir 10 x Ir 10 x Ir <10 x Ir
tsd (s) <0.2 NA
UPS rating 400 kW
  Input Bypass/Output Battery
IkPh-PE (kA) 10 9.5 NA
Voltage (V) 380 400 415 440 380 400 415 440 380-440
Breaker type
Breaker type
ComPacT NS800H MicroLogic 5.0 (3P: 33553, 4P: 33556) ComPacT NSX 630H MicroLogic 2.0
(3P: C6332D630, 4P: C6342D630)
MasterPacT NW20HDC-D MicroLogic 1.0 DC (48652+65273)
In/trip unit 800 800 800 800 800 800 630 630 2000
Io 630 630
Ir setting 0.95 0.95 0.9 0.9 0.9 0.9 1 0.94
Ir 760 760 720 720 720 720 630 592 2000
Isd/ii* <10 x In <10 x In <10 x In <10 x In 10 x In 10 x In 10 x Ir 10 x Ir <10 x Ir
tsd (s) <0.2 NA
UPS rating 450 kW
  Input Bypass/Output Battery
IkPh-PE (kA) 12 10.5 NA
Voltage (V) 380 400 415 440 380 400 415 440 380-440
Breaker type
Breaker type
ComPacT NS1000H MicroLogic 5.0

(3P: 33559, 4P: 33562)

ComPacT NS800H MicroLogic 5.0

(3P: 33553, 4P: 33556)

ComPacT NS800H MicroLogic 5.0 (3P: 33553, 4P: 33556) MasterPacT NW20HDC-D MicroLogic 1.0 DC (48652+65273)
In/trip unit 1000 1000 800 800 800 800 800 800 2000
Io
Ir setting 0.9 0.9 1 0.95 0.98 0.95 0.9 0.9
Ir 900 900 800 760 784 760 720 720 2000
Isd/ii* <8 x In <8 x In <10 x In <10 x In 10 x In 10 x In 10 x In 10 x In 2500
tsd (s) <0.2 NA
UPS rating 500 kW
  Input Bypass/Output Battery
IkPh-PE (kA) 12.5 12 NA
Voltage (V) 380 400 415 440 380 400 415 440 380-440
Breaker type
Breaker type
ComPacT NS1000H MicroLogic 5.0 (3P: 33559, 4P: 33562) ComPacT NS800H MicroLogic 5.0
(3P: 33553, 4P: 33556)
MasterPacT NW20HDC-D MicroLogic 1.0 DC (48652+65273)
In/trip unit 1000 1000 1000 1000 1000 1000 800 800 2000
Io
Ir setting 0.95 0.95 0.9 0.9 0.9 0.9 0.98 0.95
Ir 950 950 900 900 900 900 784 760 2000
Isd/ii* <8 x In <8 x In <8 x In <8 x In 8 x In 8 x In 10 x In 10 x In 2500
tsd (s) <0.2 NA

Recommended Downstream Protection for Distribution Circuit Breakers for IEC

NOTE: The recommended downstream protection for distribution circuit breakers is sized for protection of the SCRs in the static bypass switch and for coordination with the unit input breaker (UIB)/static switch input breaker (SSIB) when external backfeed protection is used.
UPS rating 200 kW 250 kW 300 kW 350 kW 400 kW 450 kW 500 kW
Breaker type
Breaker type
NSX160 NSX250 NSX400
Trip module type TM-D or Micrologic TM-D or Micrologic Micrologic
In/trip module rating ≤160 ≤250 ≤400

Recommended Cable Sizes for IEC

DANGER
hazard of electric shock, explosion, or arc flash
  • All wiring must comply with all applicable national and/or electrical codes.
  • The maximum allowable cable size is 240 mm2.
  • Shrink sleeve must be fitted over cable lug crimped zone and must overlap with the cable insulation on all power cables.
Failure to follow these instructions will result in death or serious injury.

The maximum number of cable connections per busbar:

  • 4 on input/output/bypass busbars

  • 4 x 240 mm2 on input/output/bypass busbars

  • 4 x 240 mm2 or 8 x 150 mm2 on DC+/DC- busbars

  • 8 on N busbar

  • 16 on PE busbar

NOTE: Overcurrent protection is to be provided by others.

Cable sizes in this manual are based on the minimum requirements in table B.52.3 and table B.52.5 of IEC 60364-5-52 with the following assertions*:

  • 90 °C conductors

  • An ambient temperature of 30 °C

  • Use of copper or aluminum conductors

  • Installation method F

  • Single layer on a perforated cable tray

PE cable size is based on table 54.2 of IEC 60364-5-54.

If the ambient temperature is greater than 30 °C, larger conductors are to be selected in accordance with the correction factors of the IEC.

The bypass/output cables are sized based on the nominal current +10%. This is to accommodate either low grid voltage or deviation in cable length between parallel UPSs. The DC cables are sized based on end-of-discharge voltage which has been defined as 380 VDC per IEC 60364.3 Omission of devices for protection against overload.

Copper

UPS rating 200 kW 250 kW
Voltage (V) 380 400 415 440 380 400 415 440
Input phases (mm2) 1 x 120 1 x 120 1 x 120 1 x 120 1 x 185 1 x 185 1 x 150 1 x 150
Input PE (mm2) 1 x 70 1 x 70 1 x 70 1 x 70 1 x 95 1 x 95 1 x 95 1 x 95
Bypass/output phases (mm2) 1 x 120 1 x 95 1 x 95 1 x 95 1 x 150 1 x 150 1 x 150 1 x 120
Bypass PE/output PE (mm2) 1 x 70 1 x 50 1 x 50 1 x 50 1 x 95 1 x 95 1 x 95 1 x 70
Neutral (mm2) 1 x 120 1 x 95 1 x 95 1 x 95 1 x 150 1 x 150 1 x 150 1 x 120
DC+/DC- (mm2) 1 x 185 1 x 240
DC PE (mm2) 1 x 95 1 x 120
Inverter midpoint cable for 3-wire parallel (mm2) 1 x 120 1 x 120 1 x 120 1 x 120 1 x 185 1 x 185 1 x 150 1 x 150

Copper

UPS rating 300 kW 350 kW
Voltage (V) 380 400 415 440 380 400 415 440
Input phases (mm2) 1 x 240 1 x 240 1 x 240 1 x 185 2 x 150 2 x 120 2 x 120 1 x 240
Input PE (mm2) 1 x 120 1 x 120 1 x 120 1 x 95 1 x 150 1 x 120 1 x 120 1 x 120
Bypass/output phases (mm2) 1 x 240 1 x 185 1 x 185 1 x 185 1 x 240 1 x 240 1 x 240 1 x 240
Bypass PE/output PE (mm2) 1 x 120 1 x 95 1 x 95 1 x 95 1 x 120 1 x 120 1 x 120 1 x 120
Neutral (mm2) 1 x 240 1 x 185 1 x 185 1 x 185 1 x 240 1 x 240 1 x 240 1 x 240
DC+/DC- (mm2) 2 x 150 2 x 185
DC PE (mm2) 1 x 150 1 x 185
Inverter midpoint cable for 3-wire parallel (mm2) 1 x 240 1 x 240 1 x 240 1 x 240 2 x 120 2 x 120 2 x 120 1 x 240

Copper

UPS rating 400 kW 450 kW 500 kW
Voltage (V) 380 400 415 440 380 400 415 440 380 400 415 440
Input phases (mm2) 2 x 150 2 x 150 2 x 150 2 x 150 2 x 240 2 x 240 2 x 185 2 x 150 2 x 240 2 x 240 2 x 240 2 x 240
Input PE (mm2) 1 x 150 1 x 150 1 x 150 1 x 150 1 x 240 1 x 240 1 x 185 1 x 150 1 x 240 1 x 240 1 x 240 1 x 240
Bypass/output phases (mm2) 2 x 150 2 x 150 2 x 120 1 x 240 2 x 185 2 x 150 2 x 150 2 x 150 2 x 240 2 x 240 2 x 185 2 x 150
Bypass PE/output PE (mm2) 1 x 150 1 x 150 1 x 120 1 x 120 1 x 185 1 x 150 1 x 150 1 x 150 1 x 240 1 x 240 1 x 185 1 x 150
Neutral (mm2) 2 x 150 2 x 150 2 x 120 1 x 240 2 x 185 2 x 150 2 x 150 2 x 150 2 x 240 2 x 240 2 x 185 2 x 150
DC+/DC- (mm2) 2 x 240 3 x 150 3 x 185
DC PE (mm2) 1 x 240 2 x 120 2 x 150
Inverter midpoint cable for 3-wire parallel (mm2) 2 x 150 2 x 150 2 x 150 2 x 150 2 x 240 2 x 240 2 x 185 2 x 150 2 x 240 2 x 240 2 x 240 2 x 240

Aluminum

UPS rating 200 kW 250 kW
Voltage (V) 380 400 415 440 380 400 415 440
Input phases (mm2) 1 x 185 1 x 185 1 x 185 1 x 150 1 x 240 1 x 240 1 x 240 1 x 240
Input PE (mm2) 1 x 95 1 x 95 1 x 95 1 x 95 1 x 120 1 x 120 1 x 120 1 x 120
Bypass/output phases (mm2) 1 x 150 1 x 150 1 x 150 1 x 150 1 x 240 1 x 240 1 x 185 1 x 185
Bypass PE/output PE (mm2) 1 x 95 1 x 95 1 x 95 1 x 95 1 x 120 1 x 120 1 x 95 1 x 95
Neutral (mm2) 1 x 150 1 x 150 1 x 150 1 x 150 1 x 240 1 x 240 1 x 185 1 x 185
DC+/DC- (mm2) 2 x 120 2 x 150
DC PE (mm2) 1 x 120 1 x 150
Inverter midpoint cable for 3-wire parallel (mm2) 1 x 185 1 x 185 1 x 185 1 x 150 1 x 240 1 x 240 1 x 240 1 x 240

Aluminum

UPS rating 300 kW 350 kW
Voltage (V) 380 400 415 440 380 400 415 440
Input phases (mm2) 2 x 150 2 x 150 2 x 150 2 x 120 2 x 240 2 x 185 2 x 185 2 x 150
Input PE (mm2) 1 x 150 1 x 150 1 x 150 1 x 120 1 x 240 1 x 185 1 x 185 1 x 150
Bypass/output phases (mm2) 2 x 120 2 x 120 1 x 240 1 x 240 2 x 150 2 x 150 2 x 150 2 x 150
Bypass PE/output PE (mm2) 1 x 120 1 x 120 1 x 120 1 x 120 1 x 150 1 x 150 1 x 150 1 x 150
Neutral (mm2) 2 x 120 2 x 120 1 x 240 1 x 240 2 x 150 2 x 150 2 x 150 2 x 150
DC+/DC- (mm2) 2 x 240 3 x 150
DC PE (mm2) 1 x 240 2 x 120
Inverter midpoint cable for 3-wire parallel (mm2) 2 x 150 2 x 150 2 x 150 2 x 120 2 x 185 2 x 185 2 x 185 2 x 150

Aluminum

UPS rating 400 kW 450 kW 500 kW
Voltage (V) 380 400 415 440 380 400 415 440 380 400 415 440
Input phases (mm2) 2 x 240 2 x 240 2 x 240 2 x 240 (3 x 185)* (3 x 185)* 2 x 240 2 x 240 (3 x 185)* (3 x 185)* (3 x 185)* (3 x 185)*
Input PE (mm2) 1 x 240 1 x 240 1 x 240 1 x 240 2 x 150 2 x 150 1 x 240 1 x 240 2 x 150 2 x 150 2 x 150 2 x 150
Bypass/output phases (mm2) 2 x 240 2 x 240 2 x 185 2 x 150 2 x 240 2 x 240 2 x 240 2 x 240 (3 x 185)* (3 x 185)* 2 x 240 2 x 240
Bypass PE/output PE (mm2) 1 x 240 1 x 240 1 x 185 1 x 150 1 x 240 1 x 240 1 x 240 1 x 240 2 x 150 2 x 150 1 x 240 1 x 240
Neutral (mm2) 2 x 240 2 x 240 2 x 185 2 x 150 2 x 240 2 x 240 2 x 240 2 x 240 (3 x 185)* (3 x 185)* 2 x 240 2 x 240
DC+/DC- (mm2) 3 x 185 3 x 240 4x185
DC PE (mm2) 2 x 150 2 x 185 2 x 185
Inverter midpoint cable for 3-wire parallel (mm2) 2 x 240 2 x 240 2 x 240 2 x 240 (3 x 185) (3 x 185) 2 x 240 2 x 240 (3 x 185) (3 x 185) (3 x 185) (3 x 185)

Guidance for Organizing Input, Bypass, And Output Cables

The input, bypass, and output cables must be grouped in circuits. On raceways, use one of the two shown cable formations.

Load Sharing in Bypass Operation in a Parallel System

The impedance of the bypass paths need to be controlled in a parallel UPS system. When operating in bypass mode, the parallel load sharing is determined by the total impedance of the bypass path comprising cables, switchgear, static bypass switch, and cable formation.

Parallel System – Dual Mains

NOTICE
Risk of equipment damage
To ensure correct load sharing in bypass operation in a parallel system, the following recommendations apply:
  • The bypass cables must be the same length for all UPSs.
  • The output cables must be the same length for all UPSs.
  • The input cables must be the same length for all UPSs in a single mains system.
  • Cable formation recommendations must be followed.
  • The reactance of busbar layout in the bypass/input and output switchgear must be the same for all UPSs.
If the above recommendations are not followed the result can be uneven load sharing in bypass and overload of individual UPSs.
Failure to follow these instructions can result in equipment damage.

eConversion Limits for Parallel UPS Systems

eConversion requires a minimum load percentage on the UPS for parallel UPS systems. The minimum required load percentages depend on the power cable sizes.

NOTE: For installations using the recommended cable sizes, refer to this table for the minimum load percentages: Standard eConversion Limits Based on Recommended Cable Sizes.

Standard eConversion Limits Based on Recommended Cable Sizes

UPS rating Minimum load %
200 kW 34%
250 kW 27%
300 kW 23%
350 kW 19%
400 kW 17%
450 kW 15%
500 kW 14%

The other prerequisites to use this table include:

  • The values are calculated based on the use of recommended cable sizes.

  • Installations with maximum two cables on each phase are supported.

  • The bypass and output cables must have equal length for all UPSs.


NOTE: For certain installations such as installations with 80% breakers or where other installation methods have been applied to comply with the IEC standard, it is possible that non-recommended cable sizes will be used. For installations using non-recommended cable sizes, refer to this table for the voltage rating percentages: Standard eConversion Limits Based on Non-recommended Cable Sizes.

Standard eConversion Limits Based on Non-recommended Cable Sizes

UPS rating Minimum load %
200 kW 50%
250 kW 40%
300 kW 34%
350 kW 29%
400 kW 25%
450 kW 22%
500 kW 20%

The other prerequisites to use this table include:

  • The values are calculated based on the scenario of using non-recommended cable sizes.

  • Installations with three or four cables on each phase are supported.

  • The bypass and output cables must have equal length for all UPSs.

Recommended Bolt and Lug Sizes for IEC

Cable size mm2 Bolt size Cable lug type
16 M10 x 40 mm TLK 16-10
25 M10 x 40 mm TLK 25-10
35 M10 x 40 mm TLK 35-10
50 M10 x 40 mm TLK 50-10
70 M10 x 40 mm TLK 70-10
95 M10 x 40 mm TLK 95-10
120 M10 x 40 mm TLK 120-10
150 M10 x 40 mm TLK 150-10
185 M10 x 40 mm TLK 185-10
240 M10 x 40 mm TLK 240-10
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.