990-91380L-001

UL-Specific Specifications

Upstream and Downstream Protection for UL

Preconditions for Live Swap of Power Modules

Live Swap of power modules is only allowed under the following preconditions for the UPS installation; Follow either scenario 1 or scenario 2:

Preconditions for UPS installation — scenario 1 with instantaneous override values and trip times set according to the tables below in Recommended Upstream Protection for UL Preconditions for UPS installation — scenario 2 with alternative disconnect device configurations supported with GVLOPT011 and disconnect device with ERMS mode*
Circuit breakers must have instantaneous trip time of maximum 50 ms. Circuit breakers must be installed for input (unit input disconnect device UIB) and bypass (static switch input disconnect device SSIB).
Circuit breakers must have instantaneous override values set according to the table below. Circuit breakers (UIB, SSIB) must be equipped with NEC 240.87, NFPA70E, IEEE1584, or EN51110-1 compliant ERMS mode.
Circuit breakers must be installed for input (unit input disconnect device UIB) and bypass (static switch input disconnect device SSIB). For parallel systems with three or more UPSs: Circuit breakers must be installed for the output (unit output disconnect device UOB) of each UPS. The unit output disconnect device (UOB) is sized as the static switch input disconnect device (SSIB).
For parallel system with three or more UPSs: Circuit breakers must be installed for the output (unit output disconnect device UOB) of each UPS. The unit output disconnect device (UOB) is sized as the static switch input disconnect device (SSIB). Circuit breaker (UOB) must be equipped with NEC 240.87, NFPA70E, IEEE1584, or EN51110-1 compliant ERMS mode.
Live Swap is not supported for >65kAbf installations where current limiting disconnect devices are used to protect the UPS. GVLOPT011 (Galaxy VL door switch kit) must be installed in the UPS and connected so ERMS mode is set to ON on UIB and SSIB and UOB when the front door of the UPS is opened.
  In ERMS mode, the instantaneous trip current shall be set to 5000 A or less. All time-delay settings shall be set to zero.

Schneider Electric reserves the right to remove the Live Swap label from the product front if the preconditions for scenario 1 or scenario 2 are not met.

DANGER
Hazard of electric shock, explosion, or arc flash
Only perform Live Swap of the power modules in UPS installations that follow the preconditions for scenario 1 or scenario 2.
Failure to follow these instructions will result in death or serious injury.

Recommended Upstream Protection for UL

The bypass/output disconnect devices are sized based on the nominal current +10%. This is to accommodate either low grid voltage or deviation in cable length between parallel UPSs. The battery disconnect devices are sized based on the end-of-discharge voltage which has been defined as 380 VDC.

NOTE: Overcurrent protection is to be provided by others and marked with its function.
UPS rating 200 kW 250 kW
  Input Bypass Input Bypass
Breaker type
Breaker type
LJF36400CU31X LJF36400CU31X

LJF36400CU31X

LJF36400CU31X
Ir 320 280 400 360
tr ≥4 ≥4 ≥4 ≥4
li (x In) ≤12 ≤12 ≤12 ≤12
UPS rating 300 kW 350 kW 400 kW
  Input Bypass Input Bypass Input Bypass
Breaker type
Breaker type

PJF36060CU31A

PJF36060CU31A

PJF36060CU31A

PJF36060CU31A

PJF36080CU31A PJF36060CU31A
Ir 480 420 540 480 640 540
tr ≥4 ≥4 ≥4 ≥4 ≥4 ≥4
li (x In) ≤12 ≤12 ≤10 ≤12 ≤10 ≤12
UPS rating 450 kW 500 kW
  Input Bypass Input Bypass
Breaker type
Breaker type
PJF36080CU31A PJF36080CU31A PJF36080CU31A PJF36080CU31A
Ir 720 640 800 720
tr ≥4 ≥4 ≥4 ≥4
li (x In) ≤8 ≤10 ≤8 ≤10

Recommended Cable Sizes for UL

DANGER
hazard of electric shock, explosion, or arc flash
  • All wiring must comply with all applicable national and/or electrical codes.
  • The maximum allowable cable size is 600 kcmil for input/bypass/output/neutral/ground cables.
  • The maximum allowable cable size is 500 kcmil for DC cables.
  • Shrink sleeve must be fitted over cable lug crimped zone and must overlap with the cable insulation on all power cables.
Failure to follow these instructions will result in death or serious injury.

The maximum number of cable connections per busbar:

  • 4 on input/output/bypass busbars

  • 4 x 600 kcmil on input/output/bypass busbars

  • 5 x 500 kcmil or 8 x 300 kcmil on DC+/DC- busbars

  • 8 on N busbar

  • 16 on ground busbar

NOTE: Overcurrent protection is to be provided by others.

Cable sizes in this manual are based on Table 310.15 (B)(16) of the National Electrical Code (NEC) with the following assertions*:

  • 90 °C (194 °F) conductors (75 °C (167 °F) termination)

  • An ambient temperature of 30 °C (86 °F)

  • Use of copper or aluminum conductors

If the ambient temperature is greater than 30 °C (86 °F), larger conductors are to be selected in accordance with the correction factors of the NEC.

Equipment grounding conductors (EGC) are sized in accordance with the minimum requirements in NEC Article 250.122 and Table 250.122.

NOTE: 100% rated circuit breakers for UIB, UOB, MBB, SSIB. 100% rated breakers for battery breakers.

The bypass/output cables are sized based on the nominal current +10%. This is to accommodate either low grid voltage or deviation in length between parallel UPSs. The battery cables are sized based on end-of-discharge voltage which has been defined as 380 VDC.

Copper

UPS rating 200 kW 250 kW 300 kW 350 kW 400 kW 450 kW 500 kW
Voltage (V) 480 480 480 480 480 480 480
Input phases (AWG/kcmil) 1 x 350 1 x 500 2 x 4/0 2 x 300 2 x 350 2 x 400 2 x 500
Input EGC (AWG/kcmil) 1 x 3 1 x 3 2 x 2 2 x 1 2 x 1/0 2 x 1/0 2 x 1/0
Bypass/output phases (AWG/kcmil) 1 x 300 1 x 400 1 x 600 2 x 250 2 x 300 2 x 350 2 x 400
Bypass EGC/output EGC (AWG/kcmil) 1 x 4 1 x 3 1 x 2 2 x 2 2 x 1 2 x 1/0 2 x 1/0
DC+/DC- (AWG/kcmil) (mm2) 2 x 300 2 x 400 3 x 350 3 x 400 4 x 350 4 x 400 4 x 500
DC EGC (AWG/kcmil) 2 x 1 2 x 1/0 3 x 2/0 3 x 2/0 4 x 3/0 4 x 4/0 4 x 4/0
Inverter midpoint cable for 3-wire parallel (AWG/kcmil) 1 x 350 1 x 500 2 x 4/0 2 x 300 2 x 350 2 x 400 2 x 500

Aluminum

UPS rating 200 kW 250 kW 300 kW 350 kW 400 kW 450 kW 500 kW
Voltage (V) 480 480 480 480 480 480 480
Input phases (AWG/kcmil) 1 x 500 2 x 250 2 x 300 2 x 400 2 x 500 (3 x 300)* (3 x 400)*
Input EGC (AWG/kcmil) 1 x 1 2 x 1 2 x 1/0 2 x 2/0 2 x 3/0 3 x 3/0 3 x 3/0
Bypass/output phases (AWG/kcmil) 1 x 400 1 x 600 2 x 250 2 x 350 2 x 400 2 x 500 2 x 600
Bypass EGC/output EGC (AWG/kcmil) 1 x 2 1 x 1 2 x 1/0 2 x 1/0 2 x 2/0 2 x 3/0 2 x 3/0
DC+/DC- (AWG/kcmil) (mm2) 2 x 500 3 x 300 3 x 500 4 x 350 4 x 500 5 x 400 5 x 500
DC EGC (AWG/kcmil) 1 x 2/0 3 x 3/0 3 x 4/0 4 x 4/0 4 x 250 5 x 350 5 x 350
Inverter midpoint cable for 3-wire parallel (AWG/kcmil) 1 x 500 2 x 250 2 x 300 2 x 400 2 x 500 3 x 300 3 x 400

Guidance for Organizing Input, Bypass, And Output Cables

The input, bypass, and output cables must be grouped in circuits. On raceways, use one of the two shown cable formations.

Load Sharing in Bypass Operation in a Parallel System

The impedance of the bypass paths need to be controlled in a parallel UPS system. When operating in bypass mode, the parallel load sharing is determined by the total impedance of the bypass path comprising cables, switchgear, static bypass switch, and cable formation.

Parallel System – Dual Mains

NOTICE
Risk of equipment damage
To ensure correct load sharing in bypass operation in a parallel system, the following recommendations apply:
  • The bypass cables must be the same length for all UPSs.
  • The output cables must be the same length for all UPSs.
  • The input cables must be the same length for all UPSs in a single mains system.
  • Cable formation recommendations must be followed.
  • The reactance of busbar layout in the bypass/input and output switchgear must be the same for all UPSs.
If the above recommendations are not followed the result can be uneven load sharing in bypass and overload of individual UPSs.
Failure to follow these instructions can result in equipment damage.

eConversion Limits for Parallel UPS Systems

eConversion requires a minimum load percentage on the UPS for parallel UPS systems. The minimum required load percentages depend on the power cable sizes.

NOTE: For installations using the recommended cable sizes, refer to the Standard eConversion Limits Based on Recommended Cable Sizes table for the minimum load percentages.

Standard eConversion Limits Based on Recommended Cable Sizes

UPS rating Minimum load %
200 kW 34%
250 kW 27%
300 kW 23%
350 kW 19%
400 kW 17%
450 kW 15%
500 kW 14%

The other prerequisites to use this table include:

  • The values are calculated based on the use of recommended cable sizes.

  • Installations with maximum two cables on each phase are supported.

  • The bypass and output cables must have equal length for all UPSs.

NOTE: For certain installations such as installations with 80% breakers or where other installation methods have been applied to comply with the IEC standard, it is possible that non-recommended cable sizes will be used. For installations using non-recommended cable sizes, refer to the Standard eConversion Limits Based on Non-recommended Cable Sizes table for the voltage ratings percentages.

Standard eConversion Limits Based on Non-recommended Cable Sizes

UPS rating Minimum load %
200 kW 50%
250 kW 40%
300 kW 34%
350 kW 29%
400 kW 25%
450 kW 22%
500 kW 20%

The other prerequisites to use this table include:

  • The values are calculated based on the scenario of using non-recommended cable sizes.

  • Installations with three or four cables on each phase are supported.

  • The bypass and output cables must have equal length for all UPSs.

Recommended Bolt and Lug Sizes for UL

NOTICE
risk of equipment damage
Use only UL approved compression cable lugs.
Failure to follow these instructions can result in equipment damage.

Copper

Cable size Bolt size Cable lug type (one hole) Cable lug type (two hole NEMA) Crimping tool Die
1/0 AWG M10x35mm

LCB1/0-12-X

LCC1/0-12-X

CT-930

CD-920-1/0 Pink P42

2/0 AWG M10x35mm

LCB2/0-12-X

LCC2/0-12-X

CT-930

CD-920-2/0 Black P45

3/0 AWG M10x35mm

LCB3/0-12-X

LCC3/0-12-X

CT-930

CD-920-3/0 Orange P50

4/0 AWG M10x35mm

LCB4/0-12-X

LCC4/0-12-X

CT-930

CD-920-4/0 Purple P54

250 kcmil M10x35mm

LCB250-12-X

LCC250-12-X

CT-930

CD-920-250 Yellow P62

300 kcmil M10x35mm

LCB300-12-X

LCC300-12-X

CT-930

CD-920-300 Red P66

350 kcmil M10x35mm

LCB350-12-X

LCC350-12-X

CT-930

CD-920-350 Red P71

400 kcmil M10x35mm

LCB400-12-X

LCC400-12-6

CT-930

CD-920-400 Blue P76

450 kcmil M10x35mm

LCC450-12-6

CT-930
500 kcmil M10x35mm

LCB500-12-X

LCC500-12-6

CT-930

CD-920-500 Blue P87

Aluminum

Cable size Bolt size Cable lug type (one hole) Cable lug type (two hole NEMA) Crimping tool Die
1/0 AWG M10x35mm

LAA1/0-12-5

LAB1/0-12-X

CT-930

CD-920-1/0 Pink P42

2/0 AWG M10x35mm

LAA2/0-12-5

LAB2/0-12-5

CT-930

CD-920-2/0 Black P45

3/0 AWG M10x35mm

LAA3/0-12-5

LAB3/0-12-5

CT-930

CD-920-3/0 Orange P50

4/0 AWG M10x35mm

LAA4/0-12-5

LAB4/0-12-5R

CT-930

CD-920-4/0 Purple P54

250 kcmil M10x35mm

LAA250-12-5

LAB250-12-5

CT-930

CD-920-250 Yellow P62

300 kcmil M10x35mm

LAA300-12-2

LAB300-12-2

CT-930

CD-920-300 Red P66

350 kcmil M10x35mm

LAA350-12-2

LAB350-12-2R

CT-930

CD-920-350 Red P71

400 kcmil M10x35mm

LAB400-12-2

CT-930

CD-920-400 Blue P76

500 kcmil M10x35mm

LAA500-12-2

LAB500-12-2R

CT-930

CD-920-500 Blue P87

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.