990-91380L-001

Notes on Interconnected Inverter Midpoint in Existing 3-Wire Parallel Systems

Some existing 3-wire parallel systems have the inverter midpoint of each UPS interconnected by cable in a daisy chain configuration. This is not relevant for new installations. It is possible to remove the daisy chained inverter midpoint from existing installations. Removal requires a full shutdown of the UPS system and mandatory recommissioning and start-up by Schneider Electric. Contact Schneider Electric for details.

DANGER
Hazard of electric shock, explosion, or arc flash
  • Hard-wired inverter midpoint between the UPS systems is energized even when the UPS is isolated from the parallel system and completely shut down.
  • Even if absence of voltage is measured, there can still be dangerous voltage transients on the neutral busbar.
  • Entering the I/O terminal area requires full shutdown of the entire parallel system and transfer to maintenance bypass.
Failure to follow these instructions will result in death or serious injury.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.