990-91380L-001

Installation Procedure for UPS

DANGER
Hazard of electric shock, explosion, or arc flash
The UPS must be secured against movement. Perform one of the following once the UPS is in its final position:
  • Lower the leveling feet until the casters no longer have contact with the floor, OR
  • Reinstall the front transportation bracket (870-32577) on the UPS and mount it to the floor, OR
  • Install the seismic anchoring kit.
Failure to follow these instructions will result in death or serious injury.
  1. Perform one of the following procedures:
  2. Perform one of the following procedures:
  3. Only for TNC or HRG earthing system:
  4. Perform one of the following procedures:
  5. Connect the Signal Cables.
  6. Connect the Signal Cables from Switchgear and Third-Party Auxiliary Products.
  7. Connect the External Communication Cables.
  8. Connect the Modbus Cables.
  9. Only for parallel system: Connect the PBUS Cables.
  10. Only for external synchronization: Connect the Signal Cables for External Synchronization.
  11. Option: Install the ERMS Door Switch Kit GVLOPT011 (Option).
  12. Install the Power Module(s).
  13. Add Translated Safety Labels to Your Product.
  14. Final installation.
For moving or decommissioning the UPS after installation has been completed, please see Decommission or Move the UPS to a New Location.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.