990-91380L-001

Connect the PBUS Cables

All PBUS cables shall be double insulated/jacket cable and minimum rated for 30 VDC.

It is recommended to use the PBUS cables provided by Schneider Electric (0W7995 or 0W7996).

  1. Connect the provided PBUS 1 (white) and PBUS 2 (red) cables to the PBUS ports on the UPSs.
  2. Mount termination plugs (T) in the unused connectors.

    Example of System with Three UPSs in Parallel

    NOTE: The maximum acceptable length of PBUS cable between two parallel UPSs is 75 meter (246 feet). In case of configurations with up to six GVL UPSs in parallel, the combined length of all the PBUS cables from UPS 1 to UPS 6 must not exceed 75 meter (246 feet). Cable specifications: Patch cable SSTP CAT6: 22-26 AWG stranded bare copper, 4 twisted pairs, shielded cable with copper foil. Contact Schneider Electric for more information.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.