990-91317G-037

漏电流

380/400/415 V UPS 系统 - 4 线安装、100% 负载

UPS 额定值 漏电流
20-50 kW(含 N+1 功率模块) 67 mA
60-100 kW 67 mA
反馈
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.