990-91111L-001

Install the Power Module(s)

CAUTION
Heavy load
Power modules are heavy and require two persons to lift.
  • 20 kW power module weighs 25 kg (55 lbs).
  • 50 kW power module weighs 38 kg (84 lbs).
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Always install power modules starting with the bottom position and upwards.
  1. Remove the screw in each side of the empty power module slot. Remove filler plate, if present.
  2. Push the power module into the slot.
  3. Reinstall the screw in each side of the slot.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?