Decommission or Move the UPS to a New Location
- Shut down the UPS completely – follow the instructions in the UPS operation manual.
- Lockout/Tagout all disconnect devices in the maintenance bypass cabinet/maintenance bypass panel/switchgear in the OFF (open) position.
- Lockout/Tagout all battery disconnect devices in the switchgear/battery solution in the OFF (open) position.
- Remove the front panel from the UPS.
- Lockout/Tagout the internal maintenance disconnect device IMB in the OFF (open) position.
- Remove all power modules from the UPS:
CAUTIONHeavy loadPower modules are heavy and require two persons to lift.- 20 kW power module weighs 25 kg (55 lbs).
- 50 kW power module weighs 38 kg (84 lbs).
Failure to follow these instructions can result in injury or equipment damage.- Remove the screws and push the unlock switch.
- Pull the power module halfway out. A locking mechanism prevents the power module from being pulled all the way out.
- Release the lock by pressing the release button on both sides of the power module and remove the power module.
- Install a filler plate (if available) in front of the empty power module slot.
- Store the power modules safely until reinstallation.
WARNINGrisk of equipment damage- Store the power modules at an ambient temperature of -15 to 40 °C (5 to 104 °F), 10-80% non-condensing humidity.
- Store the power modules in their original protective packaging.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
- Remove the lower front plate.
- Measure for and verify ABSENCE of voltage with a multimeter probe through the holes in the transparent cover for input, bypass, output, neutral, and DC.
- Remove the transparent cover.
- Measure for and verify ABSENCE of voltage on each input/bypass/output/DC busbar before continuing.
- Disconnect and remove all power cables from the UPS. See Connect the Power Cables or Connect the Power Cables with NEMA 2 Hole Plates for details.
- Remove the top cover.
- Disconnect and remove any signal cables from the top and the front of the UPS. For UPS system with modular battery cabinet(s): See Connect the Signal Cables from a Modular Battery Cabinet for details. For simplified 1+1 parallel UPS system: See Connect the IMB Signal Cables in a Simplified 1+1 Parallel System for details.
- For UPS system with maintenance bypass cabinet: Remove the interconnection hardware between the UPS and the maintenance bypass cabinet. See the installation manual provided with the maintenance bypass cabinet for details. Save all parts for reinstallation.
- For UPS system with adjacent battery cabinet: Remove the interconnection hardware between the UPS and the adjacent battery cabinet. See the installation manual provided with the adjacent battery cabinet for details. Save all parts for reinstallation.
- Reinstall all removed plates and covers. See Final Installation for details.
- If present, remove the seismic front anchoring bracket from the UPS. Save for reinstallation.
- If the UPS is installed on the mounting skid kit GVSOPT027, dismount the UPS from the mounting skid. See the installation manual provided with the kit for details.
- Reinstall the front panel on the UPS:
- Insert the two tabs in the bottom of the front panel in the UPS at a tilted angle.
- Reconnect the front panel strap to the UPS.
- Close the front panel and lock with the two locking knobs.
- Raise the feet of the UPS until the casters have full contact with the floor.
- You can now move the UPS by rolling it over the floor on
the casters.
WARNINGTIPPING hazard- The casters of the UPS are exclusively for transport on flat, even, hard, and horizontal surfaces.
- The casters of the UPS are intended for transport over short distances (i.e. inside the same building).
- Move at a slow pace and pay close attention on the floor conditions and the balance of the UPS.
Failure to follow these instructions can result in death, serious injury, or equipment damage. - If present, remove the rear seismic anchoring bracket from the UPS and remove the seismic anchors from the floor. Save for reinstallation. See Install the Seismic Anchoring (Option) for details.
- For transport over longer distances or in conditions
that are not suitable for the casters of the UPS:
WARNINGTIPPING hazardFor transport over longer distances or in conditions that are not suitable for the casters of the UPS, ensure:- that personnel performing the transport have necessary skills and have received adequate training;
- to use appropriate tools to safely lift and transport the UPS;
- to protect the product against damage by using appropriate protection (like wrapping or packaging).
Failure to follow these instructions can result in death, serious injury, or equipment damage.Transportation requirements:
-
Mount the UPS in a vertical position in the center of a suitable pallet with minimum pallet dimensions: 680 mm x 1040 mm (27 in x 41 in)). The pallet must be suitable for the weight of the UPS (180 kg (397 lbs) with no power modules installed).
-
Use appropriate means of fixation to mount the UPS to the pallet.
-
The original shipping pallet in combination with the original transportation brackets can be reused, if in undamaged condition.
DANGERTIPPING hazard- The UPS must be appropriately fixed to the pallet immediately after being placed on the pallet.
- The fixation hardware must be strong enough to withstand vibrations and shocks during loading, transport, and unloading.
Failure to follow these instructions will result in death or serious injury.
WARNINGUnexpected equipment behaviorDo not lift the UPS with a forklift/pallet truck directly on the frame as it may bend or damage the frame.Failure to follow these instructions can result in death, serious injury, or equipment damage. - Perform one of the following:
- Decommission the UPS, OR
- Move the UPS to a new location to install it.
- Only for installing the UPS in a new location: Follow
the installation manual to install UPS in the new location. See Installation Procedure for Single Systems, Installation Procedure for Parallel Systems, Installation Procedure for Single Marine Systems,
or Installation Procedure for Parallel Marine Systems for installation overview. Startup must only be performed by Schneider
Electric.
DANGERhAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASHStartup must only be performed by Schneider Electric.Failure to follow these instructions will result in death or serious injury.