990-91261G-001

Connect the Power Cables from an Adjacent Modular Battery Cabinet

NOTE: The equipment grounding conductor/PE cable (0W49449), the DC cables (0W49426), and the needed bolts and nuts to connect the cables are provided with the modular battery cabinet.
  1. Set the battery disconnect device BB to the open (OFF) position and disconnect the battery terminals from the front of the battery modules in the modular battery cabinet(s).
  2. Remove the front plate on the UPS.

    Front View of the UPS

  3. Connect the equipment grounding conductor/PE cable (0W49449) to the G/PE busbar in the UPS.
  4. Connect the DC cables (0W49426) to the DC busbars in the UPS.
  5. Route the equipment grounding conductor/PE cable and the DC cables from the rear of the UPS towards the front and up in the gap between modular battery cabinet 1 and the UPS.

    Rear View of the UPS

  6. Route the equipment grounding conductor/PE cable and the DC cables into modular battery cabinet 1 and connect the equipment grounding conductor/PE cable and DC cables in modular battery cabinet 1.

    Front View of Adjacent Modular Battery Cabinet 1 and the UPS

  7. Reinstall the front plate.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.