990-91261G-001

Overview of Installation Kits

Installation Kit 0M-88357

Part Used in Number of units
USB cable
960-0598
Connect the Modbus Cables. 1
150 Ohm resistor
110-0151-Z
10
Terminal connector
730-0532
2

Optional Seismic Kit GVSOPT002

Part Used in Number of units
M8 x 20 mm bolt with washer Install the Seismic Anchoring (Option). 12
Rear anchor
870-97772
1
Rear anchoring bracket
870-31131
1
Front anchoring bracket
870-31132
1
Rear connection plate
870-31554
Used for installation with an adjacent product. Follow instructions in the installation manual for the adjacent product. 1

Optional Parallel Kit GVSOPT006

0H-9255
Part Used in Number of units
PBUS1 cable 0W6268 Connect the PBUS Cables. 1
PBUS2 cable 0W6267 1
AUX switch
540-9255
Connect the IMB Signal Cables in a Simplified 1+1 Parallel System. 2
This kit contains parts for use with other UPS models which are not relevant for this installation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.