EIO0000005686.01

System Backup

After product setup, backing up the system is recommended. Prepare a commercially available USB memory with a size of 32 GB or more, to create a backup USB.

NOTE: Right after the hibernation is performed, system backup or recovery will not run properly. Perform system backup or recovery after shutting down the product.
  1. Prepare a commercially available USB memory.
  2. Create a recovery USB with the Recovery USB in the Launcher. Refer to Recovery USB.
  3. Insert the recovery USB created in step 2 into the product.
  4. Turn on the product.
  5. While the boot screen is displayed, press the [F7] key.
  6. Enter the password (default password: Pw#12345).
  7. From the following screen, select the recovery USB.
  8. Select Backup > OK.
    NOTE:
    • If the "Factory image" folder where the factory default image is stored remains in the USB under the "Other label" drive, Reset to factory status is displayed.

    • After restoring your system image in the product, the factory default image will be lost. Even if you perform Recovery USB in the Launcher, the factory default image will be no longer created in the USB.

  9. Select the disk to backup. Only C drive can be backed up. If several storage devices are shown in the dialog box, select the storage device of C drive. If there is only one storage device, the following screen does not appear and skip to step 10.
  10. Select the drive labeled "Other label", enter a file name, and select either Save or Open.
    NOTE: Do not create the backup image in the "Factory image" folder.
  11. In the confirmation screen, select OK.
  12. Backup begins.
  13. After backup is complete, the following screen is displayed. Remove the backup USB from the product, and then select Restart or Shutdown.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.