EIO0000005686.01

Buzzer

Sets the sound on/off when you perform touch-panel operations.

Default: On

NOTE: The buzzer sound is prioritized by the UEFI BIOS settings over the Launcher's Buzzer setting. Make sure the setting is Enabled in Advanced > Onboard Device > Beep On (default: Enabled). Otherwise, even if the setting for the Launcher's Buzzer is ON, the buzzer will not make a sound.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.