EIO0000005686.01

TPM

This product comes equipped with the TPM 2.0 module.

Enable or disable TPM in accordance with the laws, regulations, and standards of each country.

TPM is enabled by default.

NOTE: Enable BitLocker to make your system more secure.
  1. Turn on the product.
  2. While the boot screen is displayed, to disable TPM, press [CTRL]+[D]; to enable TPM, press [CTRL]+[E].
  3. The product is restarted.
  4. After the setting is updated, when TPM is enabled, Trusted Computing is displayed in the BIOS Advanced menu. When it is disabled, Trusted Computing is not displayed.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.