EIO0000005686.01

System Recovery

To restore the system, a recovery USB is required. Prepare a recovery USB created with Recovery USB in the Launcher. Refer to Recovery USB.

NOTE: Right after the hibernation is performed, system backup or recovery will not run properly. Perform system backup or recovery after shutting down the product.
  1. Insert the recovery USB to this product.
  2. Turn on the product.
  3. While the boot screen is displayed, press the [F7] key.
  4. Enter the password (default password: Pw#12345).
  5. Select the recovery USB.
  6. To restore the system image backed up with Recovery USB in the Launcher, select Restore > OK.
    NOTE:
    • If the "Factory image" folder where the factory default image is stored remains in the USB under the "Other label" drive, Reset to factory status is displayed.

    • Reset to factory status resets only the operating system image. It does not reset the UEFI BIOS settings.

    • After restoring your system image in the product, the factory default image will be lost. Even if you perform Recovery USB in the Launcher, the factory default image will be no longer created in the USB.

    To restore the factory default image, select Reset to factory status > OK.

  7. Select the disk to recover. If there is only one storage, the following screen does not appear and skip to step 8.
  8. If there is one wim file stored directly under "Other label", or restore the factory default, go to step 9. If there are two or more wim files stored directly under "Other label", select the "Other label" > the wim file to restore > select Open.
  9. In the confirmation screen, select OK.
  10. Recovery begins.
  11. After recovery is complete and the following screen is displayed, remove the recovery media from the product and select either Restart or Shutdown.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.