EIO0000005686.01

Recovery USB

This feature is to create a recovery USB to restore and back up the system. During the creation of the recovery USB, the operating system image at the factory default is automatically stored in the USB. With this image, you can restore the factory default image, refer to System Recovery. If you need to back up your current system, refer to System Backup.

Prepare a commercially available USB memory with a size of 32 GB or more, to create a backup USB.

  1. Disconnect all connected devices from the product.
  2. Insert a commercially available USB memory.
  3. Open the Launcher.
  4. Select the Recovery USB icon.
  5. Select the USB memory in Select a USB storage device.
  6. Select Start.
  7. In the confirmation screen, select OK.
  8. When completed, the following message appears and select OK.
  9. Close the Recovery USB screen.
  10. After the operation, the drive labeled "Other label" is create in the USB. The operating system image at the factory default is stored in the folder named "Factory image" in the drive.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.