EIO0000005686.01

UEFI BIOS Setup Menu

To enter the UEFI BIOS setup menu:

  1. Turn on the product.

  2. While the boot screen is displayed, press the [DEL] key.

  3. Enter the password (default password: Pw#12345)*1.

  4. The BIOS screen will display.

*1 Make sure you change the default password. Refer to Changing the UEFI BIOS Password.

Depending on the settings, such as Fast Boot, you may not be able to enter the BIOS setup menu using the above procedure. If that is the case, display the setup menu using the following steps.

  1. Turn on the product and start up normally.

  2. Open Settings.

  3. Select Recovery.

  4. From Advanced startup, select Restart now.

  5. Select Troubleshoot.

  6. Select Advanced options.

  7. Select UEFI Firmware Settings.

  8. Select Restart.

  9. Enter the password (default password: Pw#12345)*1.

*1 Make sure you change the default password. Refer to Changing the UEFI BIOS Password.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.