EIO0000005686.01

Main Features

Multilanguage Support

The operating system is installed with the following languages.

English (default), Japanese, French, German, Spanish, Italian, Portuguese, Russian, Swedish, Simplified Chinese and Traditional Chinese.

UEFI BIOS

This product is equipped with the UEFI BIOS. Refer to UEFI BIOS.

Launcher

Utility that displays icons for registered files, programs, and various settings, which you can start with a simple touch operation. The Launcher already includes the icons of necessary settings for this product such as Write Filter. Refer to Launcher.

Security Support

Secure Boot is enabled on this product. Additionally, as TPM comes as part of this product, it can easily support an encryption tool, BitLocker. Furthermore, by purchasing a Trellix license you can realize a more secure environment. Refer to TPM and Trellix Software.

NOTE: Enable BitLocker to make your system more secure.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.