EIO0000005686.01

Uninstallation

When uninstalling, you need to uninstall the following two applications.

  • Trellix Solidifier

  • Trellix Installer

Steps for uninstalling is as follows.

  1. Select the Settings button.
  2. Select Apps.
  3. In Apps, select Trellix Solidifier.
  4. Select Uninstall.
  5. Follow the same steps and select Trellix_Installer, and then Uninstall.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.