EIO0000005686.01

How to Create a Standard User Account

A user account with an Administrator account type should only be used when system configuration changes are required.

For normal operations, use a user account with a Standard User account type.

The following shows how to create an account with a Standard User account type.

  1. Open Settings.
  2. Select Accounts.
  3. Select Other Users.
  4. Select Add account.
  5. Enter a username and a password, and select Next.
  6. Select the user account created, and then Change account type.
  7. Select Standard User.
  8. Select Start and then the account icon.
  9. You can select the user account created.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.