EIO0000005686.01

At First Startup

The first time you start up the product, the initial settings for the operating system is executed. Connect a keyboard and mouse before powering up, then follow the on-screen instructions to define the settings.

NOTE:

This product requires the sign-in password to be set in order to reduce the risks of unauthorized access, intrusion and infection of malicious software. The conditions for the sign-in password are as follows.

No. of characters: From the usable characters below, at least 3 types and at least 8 characters are required. The sign-in password should not contain the character strings used in the account name.

Usable characters:

  • Uppercase letters of European languages (A through Z, with diacritic marks, Greek and Cyrillic characters)

  • Lowercase letters of European languages (a through z, sharp-s, with diacritic marks, Greek and Cyrillic characters)

  • Base 10 digits (0 through 9)

  • Non-alphanumeric characters (special characters): (~!@#$%^&*_-+=`|\(){}[]:;"'<>,.?/) Currency symbols such as the Euro or British Pound are not counted as special characters for this policy setting.

  • Any Unicode character that is categorized as an alphabetic character but is not uppercase or lowercase. This includes Unicode characters from Asian languages.

  • It is not possible to recover a lost username and password.

CAUTION
EQUIPMENT DAMAGE
Regardless of the Write Filter setting, do not turn off the power immediately after turning on the product.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
LOSS OF DATA
Do not turn off the power during initial setup.
Failure to follow these instructions can result in equipment damage.
NOTICE
ACCESS LOSS
Store your device's username and password information in a secure location.
Failure to follow these instructions can result in equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.