EIO0000005686.01

In-Band ECC (only Atom model)

The CPU in this product supports In-Band ECC. The following describes the procedure for enabling and disabling In-Band ECC (default: Disabled).

  1. Display the BIOS screen. Refer to UEFI BIOS Setup Menu.
  2. Select Advanced > CPU Configuration > In-Band ECC Support.
  3. Select Enabled or Disabled.
  4. Press the [F4] key.
  5. Select Yes in the Save & Exit Setup dialog box.
  6. The product is restarted.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.