EIO0000005686.01

Windows Update

For safer use of this product, use Windows Update to keep the operating system up to date. In the factory default state, the automatic security update function is disabled. For the procedure on how to enable it, refer to the following.

NOTE:
  • If Write Filter is enabled, disable the Write Filter and update the operating system.

  • For environments where security updates cannot be applied regularly, we recommend purchasing the optional Trellix license and implementing the permission list method for security protection.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.