DOCA0110EN-08

Device Physical Location

Device Locating Procedure

Step

Action

Result

1

From the Link150 menu bar, click Home.

Opens the Home webpage.

2

In the Device Physical Location section, click ON for the Identify Device toggle key.

Locates the Link150-XXYYZZ. The RS485 LED of the selected Link150- XXYYZZ blinks for 15 seconds with 1 s ON and 1 s OFF (test mode.)

NOTE: This functionality temporarily overrides the LED blinking pattern of Modbus RS485 communication (if this communication exists).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.