DOCA0110EN-08

Link150 User Interface Layout

Overview

This graphic shows the Link150 user interface layout.

A

Banner

B

Main Tabs

C

Sub Tabs

D

Display Zone

E

Action Buttons

Banner

The banner displays the following information at the top of all the pages.

Generic information

Description

User name

Name of the user who has logged in

Logout

To log out the Link150 session, click Logout or close your browser. It is recommended to log out from the Link150 gateway when it is not in use.

Main Tabs

The main tabs are:

  • Home

  • Diagnostics

  • Maintenance

  • Settings

Sub Tabs

The sub tabs display the sub menus under the selected main tab.

Action Buttons

The action buttons correspond to the selected tab.

The following table describes the interface buttons:

Button

Action

Apply Changes

Applies the changes.

Cancel Changes

Cancels the modifications to return to the last saved settings.

Reset

Resets the values to factory settings. Values in all the fields of the selected sub tab are reset to 0

Read

Allows Link150 gateway to read the Modbus registers from the selected device, according to the selected configuration.

Default

Restores the values that are manually changed in Settings > Communication > Advanced Ethernet Settings to the default values. For example, if you change the default value of Time to Live from 60 Hops to 70 Hops, clicking

Default will restore the value to 60.

Upgrade

Upgrades the Link150 firmware to the selected version, from the Maintenance tab.

Add User

Lets you add new users.

Display Zone

The display zone shows the selected sub tab in detail with all related fields.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.