DOCA0110EN-08

User Accounts

Description

The Link150 users are assigned user names and passwords. Each user belongs to a group, and each group has access rights to the Link150 webpages assigned by the Link150 administrator.

There are two pre-defined user accounts:

  • Administrator (default password is MAC address)

    NOTE: MAC address which is unique for each LINK150. Enter the MAC address of the device without colon in capital letter (For example: if the MAC address of the LINK150 is 00:80:f4:02:14:38, then password is 0080F4021438)

  • Guest (default password is Guest)

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

User Accounts Configuration Procedure

Step

Action

Result

1.

From the Link150 menu bar, click Settings.

Opens the Settings menu.

2.

From the Settings menu, in the User Management submenu, click User Accounts.

Displays the user accounts details.

3.

Click Add User and enter User Name, Password, Confirm Password and then select Role

Enters the new user account name, password, and role.

4.

Click Apply Changes.

Creates the new user account for Link150 gateway.

Users

In addition to the two default user accounts, you can create up to 10 user accounts.

Parameter

Description

User Name

Enter a name between 4 and 16 characters for a new user.

NOTE: User names is case-sensitive and white space characters are not allowed.

Password

Enter a password between 8 and 16 characters for a new user.

NOTE: Password is case-sensitive and must contain at least 1 number, 1 capital letter, and 1 special character.

Confirm Password

Re-enter a password for confirmation.

NOTE: Password is case-sensitive.

Role

Select a role for the new user.

Link150 Accounts and Passwords

Accounts

Password

Administrator

MAC address

NOTE: MAC address which is unique for each LINK150. Enter the MAC address of the device without colon in capital letter (For example: if the MAC address of the LINK150 is 00:80:f4:02:14:38, then password is 0080F4021438)

Guest

Guest

User-defined accounts (10 accounts possible)

User-defined passwords

User Account lockout policy

After the 5th consecutive invalid login attempt, the webpage login is locked for 2 minutes. After 2 minutes (expiry), the webpage is unlocked. Alternately you can perform power cycle or soft restart or factory reset to unlock the user account.

NOTE: If you perform factory reset, all user accounts except Administrator and Guest are deleted and the webpage user account goes back to factory default settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.