DOCA0110EN-08

Identification

Description

This page displays the details of Link150 gateway. The details are user application name, product range, product model, serial number, firmware revision, unique identifier.

Date and Time Configuration Procedure

Step

Action

Result

1

From the Link150 menu bar, click Settings.

Opens the Settings menu.

2

From the Settings menu, in the General submenu, click Identification.

Displays the Device Identification details.

3

Enter the Link150 gateway name in the User Application Name box, and click Apply Changes.

Changes the User Application Name (Device Name.)

Device Identification Parameters

Parameter

Description

User Application Name

Device name that is assigned by the user.

Product Range

Name of the device type.

Product Model

Device model number.

Serial number

Device serial number.

Firmware Revision

Current firmware version.

Unique Identifier

Combination of MAC address and the time.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.