DOCA0110EN-08

System Log Configuration

Configuring the system log

This page allows the user to set a system log server to receive the various log events on a specific interval.

You can choose the category and severity of events to be received.

NOTE: By default, all the Security events will be sent to the server if the service is enabled.

  1. Click Settings > Communication > System Log.

  2. Modify the parameters as required.

Parameter

Values

Description

System Log Service

Enable

-

Enable or disable the system log service.

System Log Server Settings

System Log server Address

-

Enter the server name or IP address.

Connection Mode

  • TCP/TLS

  • TCP

  • UDP

Select the mode.

System Log Server Port

1 to 65534

Enter the system log server port number.

System Log Export Settings

Export Interval

0 to 3600

NOTE: Default 60

Enter the interval duration for exporting the log data in seconds.

Export Filters

Category

  • Application

  • Security

  • System

  • Other

  • All

Select the category of the events.

NOTE: The events with category Security are always transferred irrespective of the selection in severity filters.

Severity:

  • Alert

  • Critical

  • Debug

  • Emergency

  • Error

  • Information

  • Notice

  • Warning

  • All

Select the severity of the event.

System Log Test

-

Test connection

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.