DOCA0110EN-08

Device Identification

Description

This page shows the details of Link150 gateway. The details are user application name, product range, product model, serial number, firmware revision, unique identifier, MAC address, IPv4 address, IPv6 link local address, and manufacture date.

Device Identification Procedure

Step

Action

Result

1

From the Link150 menu bar, select Settings.

Opens the Settings menu.

2

From the Settings menu, in the General submenu, click Identification.

Displays the Device Identification details.

3

Enter the Link150 gateway name in the User Application Name box, and click Apply Changes.

Changes the User Application Name (Device Name).

List of Parameters in Device Identification

Parameter

Description

User Application Name

Device name that is assigned by the user.

Product Range

Name of the device type.

Product Model

Device model number.

Serial Number

Device serial number.

Firmware Revision

Current firmware version.

Unique Identifier

Combination of MAC address and the time.

MAC Address

Unique MAC address.

IPv4 Address

Addressing scheme to specify the source and destination addresses.

IPv6 Link-local Address

Address used to communicate on the local network.

Manufacture Date

Date when the device was manufactured.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.