DOCA0110EN-08

Ethernet

Description

This page shows the Ethernet readings accumulated since the Link150 gateway was last activated. If the power to the Link150 gateway is terminated or the device is reset due to a configuration change or other event, all cumulative values are reset to 0.

Reset Procedure

Step

Action

Result

1

From the Link150 menu bar, click Diagnostics.

Opens the Diagnostics menu.

2

From the Diagnostics menu, in the Communication submenu, click Ethernet.

Displays the Ethernet statistics

3

Click Reset in the Ethernet Global Statistics section.

Resets the Link150 cumulative diagnostic data to 0.

Interpreting Ethernet Statistics

Ethernet Statistic

Description

Frames Transmitted OK

Number of frames transmitted

Frames Received OK

Number of frames received

Reception Errors

Number of errors frame during reception

Transmission Errors

Number of errors frame during transmission

Statistic Per Port

Description

Ethernet Port 1 and 2 Statistics

Link Speed

Operational speed (10 Mbps or 100 Mbit/s)

Duplex mode

Current mode of operation (full duplex or half duplex)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.