DOCA0110EN-08

Serial Port

Description

This page displays the diagnostic data for the devices connected to the serial port.

Serial Port Reset Procedure

Step

Action

Result

1.

From the Link150 menu bar, click Diagnostics.

Opens the Diagnostics menu.

2.

From the Diagnostics menu, in the Communication submenu, click Serial Port.

Displays the transmitted, received, and error messages.

3.

Click Reset.

Resets the number of messages to 0.

Serial Port Parameters

Parameter

Description

Settings

Transmitted Messages

Number of messages transmitted.

 

Received Messages

Number of messages received.

 

Error Messages

Number of error messages displayed.

 

Reset

Resets the transmitted, received, and error messages.

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.