DOCA0110EN-08

Date and Time

Description

This page allows to enter the local date and time manually.

NOTE: As there is no SNTP or RTC, the date or time needs to be reset in the event of power loss.

Date and Time Configuration Procedure

Step

Action

Result

1

From the Link150 menu bar, click Settings.

Opens the Settings menu.

2

From the Settings menu, in the General submenu, click Date/Time.

Displays the Date and Time.

3

Enter Date and Time.

Enters the current date and current time.

4

Click Apply Changes.

Updates current date and time of Link150 gateway.

Date and Time Parameters

Parameter

Description

Setting

Date(yyyy/mm/dd)

Allows you to set the present date.

Date format: yyyy/mm/dd

Time(hh:mm:ss)

Allows you to set the present time.

Time format: hh:mm:ss

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.